i.MX502 IOMUX for NOR Flash boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX502 IOMUX for NOR Flash boot

ソリューションへジャンプ
4,226件の閲覧回数
norishinozaki
Contributor V

Hello,

I'm configuring NOR Flash as boot device by looking at Table 6-9 in RM below.

pastedImage_0.png

Does this instruct that,  for NOR Flash boot, the Flash pins must be connected to the Pads specified in this table?

Then ROM code configures the IOMUXes the Pads without setting correspondent GPIO pins?

pastedImage_3.png

Does this sentence mean that we need to the configure shadowed pins by GPIO to be assingned propery to the specified Pad at reset?

pastedImage_1.png

However we don't need to configure manually for non-shadowed pins because ROM code does that.

We only need to conigure shadowed pins by GPIO.

Is this correct?

Best regards,

Nori Shinozaki

ラベル(1)
0 件の賞賛
返信
1 解決策
3,974件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
13 返答(返信)
3,975件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
3,974件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

yes it is correct, for NOR Flash boot the flash pins must be connected to

the pads specified in this table. Also non-shadowed pins are

set by ROM code, no need to additionally configure them.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,974件の閲覧回数
norishinozaki
Contributor V

Thanks Igor,

Now please explain how to configure shadowed EIM_D[0] to EPDC_D0.ALT2 as shown in the table when it's reset for NOR boot.

When I look at the IOMUXC register for EPDC_D0, the default value for MUX_MODE is 0001(GPIO[0]).

How can I set 010 for EIM_D[0]?

Also I have to set the SELECT_INPUT register to mode ALT2.

How can I do that?

pastedImage_0.png

Best regards,

Nori Shinozaki

0 件の賞賛
返信
3,974件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Nori,

there is no need for configuration of EIM_D[0]  EPDC_D0.ALT2

since NOR boot is performed on D16-D31 pads (selection

BOOT_CFG2[7:6]=01 - Not Muxed, 16-bit data (high half) interface)

EIM_DA0-15.ALT0 are for selection BOOT_CFG2[7:6]=00 - Muxed, 16-bit data (low half) interface

Shadowed pads are not used for boot.

Best regards

igor

0 件の賞賛
返信
3,974件の閲覧回数
norishinozaki
Contributor V

Hello Igor,

Thanks again,

Let me confirm the Table 23-2 below

Is these correction in red are correct?

Because...

BOOT_CFG2[7:6]=00 - Muxed, 16-bit data (low half:DA0-15) interface

From 23.101.1 EIM_CSGCR1,

     MUM=1

     DSZ=001(lower 2bits applied)

So EIM_BOOT=0x101

BOOT_CFG2[7:6]=01 - Not Muxed, 16-bit data (high half:D16-31) interface

From 23.101.1 EIM_CSGCR1,

     MUM=0

     DSZ=010(lower 2bits applied)

So EIM_BOOT=0x010

pastedImage_2.png

pastedImage_0.png

Best regards,

Nori Shinozaki

0 件の賞賛
返信
3,974件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hello Nori,

it is not necessary to use 23.101.1 EIM_CSGCR1

since iROM changes these settings as described in i.MX50 RM Boot Chapter:

NOR boot is performed on D16-D31 pads (selection

BOOT_CFG2[7:6]=01 - Not Muxed, 16-bit data (high half) interface)

EIM_DA0-15.ALT0 are for selection BOOT_CFG2[7:6]=00 - Muxed, 16-bit data (low half) interface

Shadowed pads are not used for boot. This corresponds to:

EIM_CS0GCR1[MUM] = ~BOOT_CFG2[6];

DSZ[0] = EIM_CS0GCR1[16] = ~ (BOOT_CFG2[7] | BOOT_CFG2[6]);

~igor

0 件の賞賛
返信
3,974件の閲覧回数
norishinozaki
Contributor V

Hello Igor,

Thank you!

You mean DSZ[1] isn't cared, right?

Then, EIM_BOOT can be either of following values.

#Not muxed: BOOT_CFG2[7:6] = 0x01

EIM_BOOT[2:0] = 0x000

2: MUM    = 0

1:DSZ[1] = *(say, 0)

0:DSZ[0] = 0

#Muxed: BOOT_CFG2[7:6] = 0x00

EIM_BOOT[2:0] = 0x101

2: MUM    = 1

1: DSZ[1] = *(say, 0)

0: DSZ[0] = 1

So, as long as we use Not Muxed, 16-bit data (high half) settings, we don't neet to care about the 23.101.1 EIM_CSGCR1 register. Because ROM will set it so.

In other words, we can use Muxed mode by settings EIM_BOOT[2:0] pins in 0x101.


Best regards,

Nori Shinozaki

0 件の賞賛
返信
3,974件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hello Nori,

yes, ROM sets EIM_CSGCR1 register

BOOT_CFG2[7:6]=00 - Muxed, 16-bit data (low half) interface  =>  DSZ = 001

BOOT_CFG2[7:6]=01 - Not Muxed, 16-bit data (high half) interface) =>DSZ = 010

DSZ[1] =~ (~(BOOT_CFG2[7] ^ BOOT_CFG2[6]);

~igor

0 件の賞賛
返信
3,974件の閲覧回数
norishinozaki
Contributor V

Hello Igor,

Thanks but you wanted to write

DSZ[1] =~ (~BOOT_CFG2[7] ^ BOOT_CFG2[6]);

?

Now it tuned out my customer has to use D0-15 pins to connect NOR FLASH for booting.

They need to set BOOT_CFG2[7:6]=00 by GPIO Boot Overrides as written in the Table 6-8 below

pastedImage_0.png

Then when I look at Table 6-3 to try to find out the GPIO pins but there are no "Contact" for BOOT_CFG2[7:6].

pastedImage_1.png

How can we really set BOOT_CFG2[7:6]=00?

BTW, EIM_BOOT[2:0] are internal signals generated by BOOT_CFG2[7:6]?

Best regards,

Nori Shinozaki

0 件の賞賛
返信
3,974件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hello Nori,

yes EIM_BOOT are internal signals generated by BOOT_CFG2[7:6]:

EIM_DA14  BOOT_CFG2[6]

EIM_DA15  BOOT_CFG2[7]

~igor

.

0 件の賞賛
返信
3,974件の閲覧回数
norishinozaki
Contributor V

Hello Igor,

Thanks, so the only things they need to do non-mux NOR boot,

Tie EIM_DA14 and 15 to low when reset.

Is this correct?

Nori Shinozaki

0 件の賞賛
返信
3,974件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hello Nori,

BOOT_CFG2[7:6]=01 - Not Muxed, 16-bit data (high half) interface)

EIM_DA14 = BOOT_CFG2[6]

EIM_DA15 = BOOT_CFG2[7]

~igor

0 件の賞賛
返信
3,974件の閲覧回数
norishinozaki
Contributor V

Igor,

Thanks!

Best regards,

Nori Shinozaki

0 件の賞賛
返信