Hello Champs,
I'm going to build images for i.MX50 EVK
First I did the config
./ltib -m config
In the config when I choose (imx51) Platform, I can choose a board (mx50_rd3) for u-boot as follows.
However when I choose (imx53) Platform, I can't choose anything as follows.
I guess that is a common u-boot for i.mx50, 51, 53.
Which is the best and latest option for i.MX50 EVK?
Best regards,
Nori Shinozaki
Solved! Go to Solution.
Hi Nori
one needs to select mx50_rdp as in attached file p.11
linux is L2.6.35__11.04_ER_SOURCE : Linux 2.6.35 Source
Code Files and documentation 2011.04.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX508&fpsp=1&tab=Design_Tools_Tab
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
You wrote mx50_rdp but it must be mx50_rd3 because I'm using MX50 EVK Rev D.
Correct?
Best regards,
Nori Shinozaki
Hi Nori
yes correct.
Best regards
igor