i.MX50 ./ltib -m config option for i.MX50 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX50 ./ltib -m config option for i.MX50 EVK

Jump to solution
863 Views
norishinozaki
Contributor V

Hello Champs,

I'm going to build images for i.MX50 EVK

First I did the config

./ltib -m config

In the config when I choose (imx51) Platform, I can choose a board (mx50_rd3) for u-boot  as follows.

pastedImage_4.png

However when I choose (imx53) Platform, I can't choose anything as follows.

I guess that is a common u-boot for i.mx50, 51, 53.

Which is the best and latest option for i.MX50 EVK?

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
1 Solution
728 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

yes correct.

Best regards

igor

View solution in original post

0 Kudos
3 Replies
728 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

one needs to select mx50_rdp as in attached file p.11

linux is L2.6.35__11.04_ER_SOURCE : Linux 2.6.35 Source

Code Files and documentation 2011.04.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX508&fpsp=1&tab=Design_Tools_Tab

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
728 Views
norishinozaki
Contributor V

Hi Igor,

You wrote mx50_rdp but it must be mx50_rd3 because I'm using MX50 EVK Rev D.

Correct?

Best regards,

Nori Shinozaki

0 Kudos
729 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

yes correct.

Best regards

igor

0 Kudos