i.MX353 LPDDR Bus impedance control

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX353 LPDDR Bus impedance control

Jump to solution
713 Views
Tony1z
Contributor I

Hello Sir,

I saw that i.MX Layout application note recommends to control single-ended impedance 50 Ohms on LPDDR bus.

If my PCB stackup and trace width are limited, can I use lower single-ended impedance (45 Ohms for example) on LPDDR bus ?

Is lower single-ended impedance better for LPDDR bus ?

Best regards,

Tony Lin

Tags (2)
0 Kudos
1 Solution
553 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Tony,

This is the thing: PCB trace impedance has to match the output impedance of the i.MX pins, which is configurable through the DSE bits in the IOMUX registers. So for example, please take a look to table 4-5 of the reference manual. Depending on the DDR type you are using, you have different options of output pin drive strength, so if you choose 45 High drive strength for mobile DDR, the equivalent impedance is 45 Ohms, so your trace in the PCB has to have this impedance. If the impedances match, the power transfer is maximum and you won't have reflexions in your signal, this is done for signal integrity.

Hope this helps!

Best regards.

Jorge.

View solution in original post

0 Kudos
2 Replies
554 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Tony,

This is the thing: PCB trace impedance has to match the output impedance of the i.MX pins, which is configurable through the DSE bits in the IOMUX registers. So for example, please take a look to table 4-5 of the reference manual. Depending on the DDR type you are using, you have different options of output pin drive strength, so if you choose 45 High drive strength for mobile DDR, the equivalent impedance is 45 Ohms, so your trace in the PCB has to have this impedance. If the impedances match, the power transfer is maximum and you won't have reflexions in your signal, this is done for signal integrity.

Hope this helps!

Best regards.

Jorge.

0 Kudos
553 Views
Tony1z
Contributor I

Hi Jorge,

Thanks for your explanation. It helps me.

Best regard,

Tony

0 Kudos