i.MX35 QSB: Update to BSP 11.09 breaks FullHD playback?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX35 QSB: Update to BSP 11.09 breaks FullHD playback?

811件の閲覧回数
WolfgangW
Contributor I

Hi,

I just updated my i.MX35 QSB microSD using the new packages from the 11.09 BSP release, and FullHD playback stopped working now.

I can play back some 720p material I have, but none of the 1080p clips do work.

 

Below is what I get as output. Did anybody else try upgrading and had similar problems? Is this a known issue (did not find anything concerning this, though), or was 1080p disabled due to memory bandwidth limitations?

(The  "socket(): Address family not supported by protocol" was there before, too, and did not cause any problems, so seems to be unrelated.)

 

Any hints what I might be doing wrong are appreciated!

 

Thank you,

Wolfgang

 

lucid@lucid-desktop:~$ gst-launch playbin2 uri=file:///mnt/test/big_buck_bunny_1080p_h264.mp4
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
Aiur: 2.0.3-1-179-e630aa8d
Core: MPEG4PARSER_06.04.04 build on Sep 27 2011 09:56:41
mime: video/quicktime; audio/x-m4a; application/x-3gp
file: lib_mp4_parser_arm11_elinux.3.0.so.6.4.3
Content Info:
URI:
file:///mnt/test/big_buck_bunny_1080p_h264.mp4
Idx File:
/home/lucid/.aiur/.mnt.test.big_buck_bunny_1080p_h264.mp4.aidx
Seekable : Yes
Size(byte): 725106140

Movie Info:
Seekable : Yes
Live : No
Duration : 0:09:56.461696000
ReadMode : File
Track : 3

Track 00[Video]: Enabled
Duration: 0:09:56.458304000
Language: und
Mime:
video/x-h264, parsed=(boolean)true, width=(int)1920, height=(int)1080, framerate
=(fraction)24/1
H264D_ARM11_02.06.01 build on Jul 12 2011 13:38:27.
MFW_GST_H264_DECODER_PLUGIN 2.0.3-1-179-e630aa8d build on Sep 28 2011 15:41:58.
Track 01[Text]: Disabled
Codec: 0, SubCodec: 0
Track 02[Audio]: Enabled
Duration: 0:09:56.480000000
Language: und
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)6, rate=(int)48000, bitrate=(int)4
48000, framed=(boolean)true
BLN_MAD-MMCODECS_AACD_ARM_03.06.00 build on May 9 2011 17:11:11.
MFW_GST_AAC_PLUGIN 2.0.3-1-179-e630aa8d build on Sep 28 2011 15:04:33.
MFW_GST_V4LSINK_PLUGIN 2.0.3-1-179-e630aa8d build on Sep 28 2011 15:04:02.
socket(): Address family not supported by protocol
ERROR: from element /GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/MFW_GST_H264DEC_INFO_T:mfw_gst_h264dec_info_t0: fatal error
Additional debug info:
non recoverable error while decoding the H.264 Data
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Total rendered:0
[--->FINALIZE v4l_sink
[--->FINALIZE aiurdemux
Freeing pipeline ...

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

583件の閲覧回数
WolfgangW
Contributor I

Sorry,

the edit did not get through.

Clock problem is also only present when not running as root. sudo gst-launch... works correctly.

 

Apart from FullHD still being a bit jerky (no thorough investigation done yet - video is still played as an overlay, which I suspect to be the problem due to memory bandwidth), the update really is a great step forward.

Thanks for the great work!

 

Regards,

Wolfgang

0 件の賞賛
返信

583件の閲覧回数
WolfgangW
Contributor I

Hi again,

seems ito be partially solved - I could get my "standard" test clip to work when running gst-launch as superuser (sudo gst-launch ...). This does not help for big buck bunny, but thinking about it I am not sure if I tried it before on this platform.

However, there still seem to be new problems as with some clips I get this warning that was not present before:


WARNING: from element /GstPlayBin2:playbin20: Internal GStreamer error: clock problem. Please file a bug at http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer.
Additional debug info:
gstbin.c(2308): gst_bin_do_latency_func (): /GstPlayBin2:playbin20:
Failed to configure latency of 0:00:00.000000000

 

Playback is too slow in this case. Sorry, I can't provide the files as it is customer material. This is the info I get from gstreamer, in case it helps:

Movie Info:
Seekable : Yes
Live : No
Duration : 0:03:00.836992000
ReadMode : File
Track : 2

Track 00[Video]: Enabled
Duration: 0:03:00.800000000
Language: eng
Mime:
video/x-h264, parsed=(boolean)true, width=(int)1280, height=(int)720, framerate=
(fraction)25/1
H264D_ARM11_02.06.01 build on Jul 12 2011 13:38:27.
MFW_GST_H264_DECODER_PLUGIN 2.0.3-1-179-e630aa8d build on Sep 28 2011 15:41:58.
Track 01[Audio]: Enabled
Duration: 0:03:00.836992000
Language: eng
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)44100, bitrate=(int)1
59421, framed=(boolean)true



Regards,

Wolfgang

0 件の賞賛
返信