i.MX35 IPU image rotation for 90 degree cannot be realized

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX35 IPU image rotation for 90 degree cannot be realized

1,938件の閲覧回数
ruitan
Contributor II

Hi,

     I am using i.MX353 processor WITHOUT Linux. My purpose is to rotate an image (the data had stored in an one dimensional array) for 90 degree.

     I have done some necessary steps as the user's manual asks, which are as following:

     [1] Referred 31.4.2.5 Rotation Section;

     [2] Referred 31.4.8.2 Frame Synchronization Unit (FSU), The “MEM --> IC (ROT ENC) --> MEM”  task chain in “Table 31-166. Programming IPU Flows and Tasks (Continued) ”, and followed with the “Manual on input, manual on output” config method;

     [3] In register IDMAC_CHA_EN, enabled DMAIC8 and DMAIC10;

     [4] In register IPU_CONF, enabled rotation unit, IC interface, CSI interface;

     [5] In register IC_CONF, disabled PRPENC_EN, RWS_EN, CSI_MEM_WR_EN;

     [6] In register IPU_FS_PROC_FLOW, disabled PRPENC_ROT_SRC_SEL;

     [7] In register IC_CONF, enabled PRPENC_ROT;

     [8] Trigger the IC encoding rotation task by setting '1' on DMAIC_8_BUF0_RDY and DMAIC_10_BUF0_RDY.

     In the program, I created two one dimensional arrays(type: unsigned char, size: 1280*960), one for DMAIC8 and another for DMAIC10. After the rotation task has been triggered, the IPU_TASKS_STAT register shows that ENC_ROT_TSTAT was ACTIVE. However, I waited very long but ENC_ROT_TSTAT was still ACTIVE, no data received in the DMAIC10 array.

     Could anyone tell me how to make this rotation 90 degree work? Thank you!

Rui

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,353件の閲覧回数
ruitan
Contributor II

oh, btw, my image type is grayscale image with a byte per pixel.

0 件の賞賛
返信

1,353件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello,

I think you are doing the steps fine, let me share with you an example of  an i.MX31 which has the same IPU.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信