i.MX31L(MCIMX31LDVKN5D) absolute maximum rating

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX31L(MCIMX31LDVKN5D) absolute maximum rating

488 Views
hirosuzu
Contributor I

I have a question about I.MX31L(MCIMX31LDVKN5D).

When a DDR output overshoot or undershoot,

is a maximum or a minimum voltage of the DDR output equal to

an absolute maximum rating of I.MX31L?

(Input Voltage Range Vimax:-0.5V(min)、NVcc 0.3V(=1.8 0.3=2.1V)

Tags (1)
0 Kudos
Reply
1 Reply

413 Views
Yuri
NXP Employee
NXP Employee

  You are right, the fact, that over-/under-shoots voltages are not specified
means that :


No overshoot above max voltage specified is allowed (NVCC2x+0.3V)

No undershoot below min specified is allowed (-0.3 V)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply