i.MX28EVK WINCE Image destroyed - help?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX28EVK WINCE Image destroyed - help?

843件の閲覧回数
ReinhardMeyer
Contributor II

Hi,

I accidentially crashed my SD Card with WinCE for the i.MX28EVK be removing the card

while the system was running (I did not expect this to be a problem).

It appears that at least Block 0 has been zeroed out. Since I use WinCE for Demo

only I would prefer to download just the raw image and not tools, whistles and bells

to reconstruct it.

(I can easyly do a dd if=<image> of=/dev/sdb on any Linux system - I should have done

the reverse before using the CE too much ;)

 

Thanks,

Reinhard

ラベル(1)
0 件の賞賛
返信
0 返答(返信)