i.MX287_evk attaching mtd1 to ubi0 failed

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX287_evk attaching mtd1 to ubi0 failed

Jump to solution
338 Views
hwo
Contributor III

Kernel version is 2.6.35.3, and the board has a ST micro nand flash, totally 64MB(512+16 per page).

But when I burn the board, it fails to attach mtd1 to ubi0 subsystem. Here is the debug trace:

i.MX GPMI NFC

NFC: Version 1, 8-chip GPMI and BCH

Boot ROM: Version 1, Single-chip boot area, block mark swapping supported

Scanning for NAND Flash chips...

NAND device: Manufacturer ID: 0x20, Chip ID: 0x76 (ST Micro NAND 64MiB 3,3V 8-bit)

-----------------------------

NAND Flash Device Information

-----------------------------

Manufacturer      : ST Micro (0x20)

Device Code       : 0x76

Cell Technology   : SLC

Chip Size         : 64 MiB

Pages per Block   : 32

Page Geometry     : 512+16

ECC Strength      : 8 bits

ECC Size          : 512 B

Data Setup Time   : 35 ns

Data Hold Time    : 15 ns

Address Setup Time: 0 ns

GPMI Sample Delay : 6 ns

tREA              : Unknown

tRLOH             : Unknown

tRHOH             : Unknown

Description       : NAND512W3A2

-----------------

Physical Geometry

-----------------

Chip Count             : 1

Page Data Size in Bytes: 512 (0x200)

Page OOB Size in Bytes : 16

Block Size in Bytes    : 16384 (0x4000)

Block Size in Pages    : 32 (0x20)

Chip Size in Bytes     : 67108864 (0x4000000)

Chip Size in Pages     : 131072 (0x20000)

Chip Size in Blocks    : 4096 (0x1000)

Medium Size in Bytes   : 67108864 (0x4000000)

------------

NFC Geometry

------------

ECC Algorithm          : BCH

ECC Strength           : 8

Page Size in Bytes     : 528

Metadata Size in Bytes : 10

ECC Chunk Size in Bytes: 512

ECC Chunk Count        : 1

Payload Size in Bytes  : 512

Auxiliary Size in Bytes: 16

Auxiliary Status Offset: 12

Block Mark Byte Offset : 502

Block Mark Bit Offset  : 0

-----------------

Boot ROM Geometry

-----------------

Boot Area Count            : 1

Boot Area Size in Bytes    : 20971520 (0x1400000)

Stride Size in Pages       : 64

Search Area Stride Exponent: 2

Scanning device for bad blocks

Boot area protection is enabled.

Creating 2 MTD partitions on "gpmi-nfc-main":

0x000000000000-0x000001400000 : "gpmi-nfc-0-boot"

0x000001400000-0x000004000000 : "gpmi-nfc-general-use"

UBI: attaching mtd1 to ubi0

UBI: physical eraseblock size:   16384 bytes (16 KiB)

UBI: logical eraseblock size:    15360 bytes

UBI: smallest flash I/O unit:    512

UBI: VID header offset:          512 (aligned 512)

UBI: data offset:                1024                                                         <------------------------------------burn process stops here

according to the setup, BCH page layout is:

PAGE_SIZE = 528

META_SIZE = 10

DATA0_SEIZE = 512

ECC0 = 4

DATAN_SIZE = 512

ECCN = 4

NBLOCKS = 0

, which I think is OK.

So, what's the possible reason for attaching mtd fails? Wrong configuration of nand flash?

Labels (2)
0 Kudos
1 Solution
160 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi h k

recommended to use nands with 2K,4K  page

sizes as nand with 512B is not supported by gpmi driver. References

to it can be found in BSP reference manual (i.MX28_Linux_BSP_RM.pdf)

sections 2.3.8.1 (GPMI/NAND) and 14.2.2 (Error Correction) for details.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
161 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi h k

recommended to use nands with 2K,4K  page

sizes as nand with 512B is not supported by gpmi driver. References

to it can be found in BSP reference manual (i.MX28_Linux_BSP_RM.pdf)

sections 2.3.8.1 (GPMI/NAND) and 14.2.2 (Error Correction) for details.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos