i.MX28 u-boot vs. bootlets - VDD5V Source Only

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 u-boot vs. bootlets - VDD5V Source Only

Jump to solution
7,240 Views
rabryn
Contributor III

I'm bringing up a custom i.MX283 based board.  I'm having trouble with random lockups anywhere from 1 or 2 seconds to several minutes after applying power.  I believe the issue is power related.  I've implemented the design detailed in section 4.1.2.1 (VDD5V source only) of application note AN4199:

http://www.freescale.com/files/32bit/doc/app_note/AN4199.pdf

After researching the problem I came across this patch on the Freescale website:

Linux patch to add more robust support for a VDD5V or DCDC_BATT only

Currently, I'm using mainline kernel version 3.8.3 with u-boot version v2012.10.

Are the fixes described in the bootlet patch implemented in mainline u-boot?  Can u-boot be configured for VDD5V only?  I've looked into the u-boot and bootlet code, but the code is seemingly quite different...

Thanks,

Ryan

Labels (1)
1 Solution
2,755 Views
rabryn
Contributor III

Hi Fabio,

The problem is u-boot's configuration of the low-level blocks of the power management unit in a 5V only scenario as defined in section 4.1.2 of the application note linked to in the original post.  Late yesterday I was able to prove this by porting over the patched bootlet code into u-boot.  It appears u-boot's SPL implementation is based on Freescale's original bootlet code.  However, Freescale has released a 5V only patch to the bootlet code that has never made it into u-boot.

I now have a working system.  Over time I'll try and clean up my modifications to u-boot and get some kind of patch together.

Thanks,

Ryan

View solution in original post

0 Kudos
34 Replies
635 Views
gonfer
Contributor V

In September I made some trials with Yocto. I've just run the evk with one of these images, core-image-minimal, and I see the same behaviour (U-boot 2014.01):

HTLLCL0x8050100b

HTLLCL0x8050100b

0x80502008

15 to 20 seconds gap

          HTLLCLLC

U-Boot 2014.01 (Sep 26 2014 - 16:02:01)

CPU:  Freescale i.MX28 rev1.2 at 454 MHz

BOOT:  SSP SD/MMC #0, 3V3

DRAM:  128 MiB

NAND:  128 MiB

MMC:  MXS MMC: 0

*** Warning - bad CRC, using default environment

I'm going to try 2014.10

Thanks,

Gonzalo.

0 Kudos
635 Views
gonfer
Contributor V

Same behaviour using U-Boot 2014.10

HTLLCL0x8050100b

HTLLCL0x8050100b

0x80502008

          HTLLCLLC

U-Boot 2014.10-dirty (Oct 17 2014 - 16:06:40)

CPU:   Freescale i.MX28 rev1.2 at 454 MHz

BOOT:  SSP SD/MMC #0, 3V3

SPI:   ready

DRAM:  128 MiB

NAND:  128 MiB

MMC:   MXS MMC: 0

*** Warning - bad CRC, using default environment

Thanks,

Gonzalo

0 Kudos
635 Views
fabio_estevam
NXP Employee
NXP Employee

Boots fine here for me:

HTLLCLLC                                                                  
                                                                          
U-Boot 2014.10-rc1-16572-g080d72f (Aug 21 2014 - 18:13:55)                
                                                                          
CPU:   Freescale i.MX28 rev1.2 at 454 MHz                                 
BOOT:  SSP SD/MMC #0, 3V3                                                 
SPI:   ready                                                              
DRAM:  128 MiB                                                            
NAND:  0 MiB                                                              
MMC:   MXS MMC: 0                                                         
Video: MXSFB: 'videomode' variable not set!                               
In:serial                                                             
Out:   serial                                                             
Err:   serial                                                             
Net:   FEC0 [PRIME], FEC1                                                 

Hit any key to stop autoboot:  0  

0 Kudos
635 Views
gonfer
Contributor V

Fabio,

how is your switch S16 set up? can you try with S16 set to USB_5V?

Thanks,

Gonzalo.

0 Kudos
635 Views
fabio_estevam
NXP Employee
NXP Employee

S16 is at "Wall 5V". If I put it to "USB 5V" then it does not boot.

0 Kudos
635 Views
gonfer
Contributor V

Thanks for your test. In my test, if S16 at

- Wall_5V: it works fine, as you've reported.

- USB_5V: You have to press the POWER button to start the board. The behaviour is the one described in my previous posts.

I think that S16 at USB_5V is the correct way to simulte operation under battery using mains supply instead of a battery. Do you agree?

Thanks,

Gonzalo.

0 Kudos
635 Views
fabio_estevam
NXP Employee
NXP Employee

If you are interested in powering the system with a battery you can connect a battery into J85 battery connector.

0 Kudos
635 Views
gonfer
Contributor V

Hi Fabio,

no, I don't consider battery operation; my project (as this thread) is VDD5V source  only.

But I found this issue with U-Boot and I didn't realized I had my evk in "battery source only". Hopefully, I haven't been able to reproduce the problem in VDD5V source only, so looks it's only related to battery operation.

Thanks for your support,

Gonzalo

0 Kudos
635 Views
fabio_estevam
NXP Employee
NXP Employee

Ok, got it. It seems things are working properly at your side then.

0 Kudos
635 Views
fabio_estevam
NXP Employee
NXP Employee

Ok, I can boot with S16 at USB 5V if I remove the wall power supply, then power the board via USB (J82) and set the S3 jumper to ON.

0 Kudos
642 Views
LeonardoSandova
Specialist I

Hi Ryan, Are you using LTIB for your development? Also, Try to do your changes using the latest BSP (L2.6.35_1.1.0_130130).

Leo

0 Kudos
642 Views
rabryn
Contributor III

I have more information about this issue.  I've come to the conclusion that u-boot is broken for iMX28 designs that implement section 4.1.2.1 of AN4199 (see my first post for more info).  If I apply the previously mentioned patch to the Freescale bootlet code I see a solid 1V8 rail on my DDR for instance, u-boot does not properly initialize the rail voltages in this configuration.  Here's an oscope screen shot of the 1V8 when u-boot initializes the power supply...

tek00001.png

I've modified u-boot/arch/arm/cpu/arm926ejs/mxs/spl_power_init.c to force the iMX28 to use the 5V supply like the following but no luck (removed battery check and battery brown out initialization). 


static void mxs_power_configure_power_source(void)

{

        struct mxs_power_regs *power_regs =

                (struct mxs_power_regs *)MXS_POWER_BASE;

        struct mxs_lradc_regs *lradc_regs =

                (struct mxs_lradc_regs *)MXS_LRADC_BASE;


        mxs_src_power_init();


        /* 5V source detected, bad battery detected. */

        writel(LRADC_CONVERSION_AUTOMATIC,

                        &lradc_regs->hw_lradc_conversion_clr);

        clrbits_le32(&power_regs->hw_power_battmonitor,

                        POWER_BATTMONITOR_BATT_VAL_MASK);


        mxs_5v_boot();


        mxs_power_clock2pll();


        mxs_switch_vddd_to_dcdc_source();

}

If anyone has any suggestions as to how to fix this issue I'd be happy to try them.

0 Kudos
642 Views
fabio_estevam
NXP Employee
NXP Employee

Ryan,

Just to make sure I understand: if you apply the 5V patches into the bootlets code, and then launch the kernel via bootlets: you don't see any lockups in this case?

0 Kudos
642 Views
rabryn
Contributor III

Fabio,

Yes, you are correct.  More importantly though, if I apply the patch to the bootlet code I see a solid 1V8 on my DDR2 rail... the thrashing you see in the oscope screenshot above is gone.

Ryan

0 Kudos