Hi,
I'm working with the i.MX28 quick start board, Ubuntu 10.04 and L2.6.35_10.12.01 LTIB. First I want to write the Linux kernel into a SD card with the mk_mx28_sd script. I have set LTIB options like explained in the i.MX28_Linux_BSP_UG document. The result of the Linux boot is attached in the txt file, that show how the boot stops and loop like below:
Starting inetd:
starting pid 1153, tty '': '/sbin/getty -L ttyAM0 115200 vt100'
process '/sbin/getty -L ttyAM0 115200 vt100' (pid 1153) exited. Scheduling for restart.
starting pid 1154, tty '': '/sbin/getty -L ttyAM0 115200 vt100'
process '/sbin/getty -L ttyAM0 115200 vt100' (pid 1154) exited. Scheduling for restart.
starting pid 1155, tty '': '/sbin/getty -L ttyAM0 115200 vt100'
process '/sbin/getty -L ttyAM0 115200 vt100' (pid 1155) exited. Scheduling for restart.
starting pid 1156, tty '': '/sbin/getty -L ttyAM0 115200 vt100'
process '/sbin/getty -L ttyAM0 115200 vt100' (pid 1156) exited. Scheduling for restart.
starting pid 1157, tty '': '/sbin/getty -L ttyAM0 115200 vt100'
ecc..
Please, help me!
Best regards!!!