i.MX28: aplay fails after playing a WAV file many times

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX28: aplay fails after playing a WAV file many times

2,809 次查看
PeterChan
NXP Employee
NXP Employee

In i.MX28, if we create a loop to use aplay to play a wav, the playback will fail eventually and report this error "aplay: pcm_write:1262: write error: Input/output error". This is a software defect in i.MX28 BSP L2.6.35_10.12.01. Please apply the attached patch to resolve this problem.

Original Attachment has been moved to: ENGR40464722-1-2-3.patch.zip

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,557 次查看
xsdfsdfsdf
Contributor I

Hi Peter,

It seems like this link is broken. Is there an alternate link through which I can get the patch?

Thanks

0 项奖励
回复