i.MX28: aplay fails after playing a WAV file many times

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28: aplay fails after playing a WAV file many times

1,894 Views
PeterChan
NXP Employee
NXP Employee

In i.MX28, if we create a loop to use aplay to play a wav, the playback will fail eventually and report this error "aplay: pcm_write:1262: write error: Input/output error". This is a software defect in i.MX28 BSP L2.6.35_10.12.01. Please apply the attached patch to resolve this problem.

Original Attachment has been moved to: ENGR40464722-1-2-3.patch.zip

Labels (1)
0 Kudos
1 Reply

642 Views
xsdfsdfsdf
Contributor I

Hi Peter,

It seems like this link is broken. Is there an alternate link through which I can get the patch?

Thanks

0 Kudos