Dear all,
We have planned USB bus powered device using i.MX28.
The product does not have a power switch.
Since it connected with USB-HOST, it begins boot.
Though we are going to design according to "VDD5V source only" of AN4199, it is not known how we should do a PSWITCH pin.
Is what is necessary just to tied to VDD3V3 or GND?
Best Regards,
George
已解决! 转到解答。
There is no need for a POWER button in a 5V only configuration. If a
5V source is present on the VDD5V pin, the i.MX device will automatically
power up. In such case the PSWITCH should be pulled down.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi guys,
I'm working on a custom i.mx28 board powered just by external 5v of USB bus. After several bootup starts of u-boot-2011.12 I found out that the system hangs on mx28_power_setup_5v_detect() function. Have you applied different tunings during spl code of u-boot? Could you give me any tips?
Regards,
Francesco
There is no need for a POWER button in a 5V only configuration. If a
5V source is present on the VDD5V pin, the i.MX device will automatically
power up. In such case the PSWITCH should be pulled down.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------