Hi,
I used IMX_MFG_TOOL to program nand flash for i.MX28.
Connected - i.MX28 EVK Board Connected using USB-OTG to PC. PC detected it as HID complaint Device and i am successfully able to
update the nand flash using IMX_MFG_TOOL. Now, when i connect my customized i.MX28 hardware Board (similar to EVK Board), PC detects it as
Unknown device though i use same device driver supplied in IMX_MFG_TOOL software.
I followed these steps (on customized hardware),
Result - PC detects my customized board as Unknown device.
my question is am i missing any step or configuration, which is there in EVK Board and not on my customized Board, Or is it something else?
Any help would be appreciated, Thanks in advance.
已解决! 转到解答。
It might work, but I’m not sure as I never tried it like that. I think zImage for “Manufacturing Firmware” profile also has some options enabled that are required for proper operation and it could be much bigger than what is really needed. So probably makes sense to do have a separate LTIB setup for updater firmware binary.
Does your customized board work otherwise? Have you verified it powers on properly etc.? This may be caused by i.MX28 not being powered on properly, and thus internal ROM is not executed (to initialize device and USB connection for programming).
Thanks for reply....Now i PC can detect it as HID complaint device. But when i try to program NAND flash using IMX_MFG_TOOL, it exits with an error saying device not connected. Below is the log for the session.
Thursday, December 06, 2012 15:57:00
1 - Panel A Start processing Singlechip NAND <LIST/>.1 - Panel A Start <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="60" onError="" text="Booting update firmware.".1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="60" onError="" text="Booting update firmware." SUCCESS code=0.1 - Panel A Start <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting update firmware.".1 - Panel A DoBoot() - Failed to load updater_ivt.sb to Recovery mode device. (err=1167)1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting update firmware." FAIL code=1167.Panel A: Updater Error 0x48f (1167) - The device is not connected.2 - Panel A Finished processing Singlechip NAND <LIST/> : FAIL code=1167.
Also, there is MT29F4G08ABADAWP which is 4GB NAND on EVK Board, Whereas i am having MT29F1G08ABADAWP which is 4GB NAND. Please suggest me, where am i going wrong...
Hi there, I came across a similar problem. Basically, for my customized board with iMX280, I am unable to connect the iMX280 USB to a PC in USB recovery mode. The PC detects it as an unknown device. By probing the D+ line, I can see it is pulled high by iMX280 for 240ms, then goes low with a packet of 68ms. But nothing happens after that and eventually and the D+ line stays low. After a while, the D+ line goes high again and stay high.
The power rails seems to be okay as compared to the iMX28 EVK.
I can see you have the same problem initially (USB unknown device). How do you get it resolved?
Hi Fernando,
I have resolved the issue. What happened to my board is, we added a USB upstream terminator between the iMX280 USB controller and the USB connector. This USB upstream terminator is the problem. After removing it and wiring the D+ and D- line directly to the USB connector, the problem is fixed and iMX280 can be detected in USB recovery mode using the factory tool.
Best Regards,
Dong
Hi Dong,
Thank you very much for answering me. So you removed all the resistors from the USB circuit (Rs's and the R to Vbus), and the ESD protections as well??
Many thanks again. BR,
Fernando
El 13/02/2013, a las 23:07, Dong Hui escribió:
i.MX28 USB-OTG problem
created by Dong Hui in i.MX Community - View the full discussion
Hi Fernando,
I have resolved the issue. What happened to my board is, we added a USB upstream terminator between the iMX280 USB controller and the USB connector. This USB upstream terminator is the problem. After removing it and wiring the D+ and D- line directly to the USB connector, the problem is fixed and iMX280 can be detected in USB recovery mode using the factory tool.
Best Regards,
Dong
Reply to this message by replying to this email -or- go to the message on Freescale Community
Start a new discussion in i.MX Community by email or at Freescale Community
First of all, you don't need 1.5K pull-up on D+ line to Vbus. This is built into iMX280.
Secondly, what I found is, the resistance (~22R) and capacitances (~30pF) which behaves as the EMI filter on the D+ and D- lines, would cause the USB interface to fail (signal distortion).
Lastly, ESD protection is still required. Just use the same one or similar one in the reference design.
I am able to see the debug prints your talking about in EVK only,but i am not able to see it on customized board. Also i have attached the log of USBanalyzer report for communication between PC to EVK and PC to my board. Please let me know if it is informative.
Why are you not able to see debug prints on your own i.MX28 board - no debug serial port or it doesn't work?
Have you modified MfgTool updater firmware so that it can run on your board? MfgTool load small linux kernel (updater firmware) to target board (i.MX28EVK or your own custom board) so it can do the programming. Default updater firmware works on i.MX28EVK, but may not work on your own board (for example, if different memory is used) and needs to be built from LTIB (there's an option for that).
Debug prints are enabled on my Board, but i am not getting any debug prints in this case, i am unable to figure out why?
I'll try to build my firmware for my board, and get back to you with the results.
Thanks.
I tried to generate mfgtool firmware using LTIB (for my kernel source) and got some success. Log is attached below:
Tuesday, December 11, 2012 20:39:01
1 - Panel A Start processing Singlechip NAND <LIST/>.
1 - Panel A Start <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="60" onError="" text="Booting update firmware.".
1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="60" onError="" text="Booting update firmware." SUCCESS code=0.
1 - Panel A Start <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting update firmware.".
1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting update firmware." SUCCESS code=0.
1 - Panel A Start <CMD/> type="push" body="mknod class/mtd,mtd0,/dev/mtd0" file="" timeout="10" onError="" text="".
looks like there is a timeout happening, while it detects the update, is it not able to detect NAND on board ? Still not getting any debug prints. Thanks.
The updated log is as follows :
Tuesday, December 11, 2012 20:34:40
1 - Panel A Start processing Singlechip NAND <LIST/>.
1 - Panel A Start <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="60" onError="" text="Booting update firmware.".
1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="60" onError="" text="Booting update firmware." SUCCESS code=0.
1 - Panel A Start <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting update firmware.".
1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting update firmware." SUCCESS code=0.
1 - Panel A Start <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="".
1 - Panel A Finished <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="" FAIL code=-65536.
Panel A: Updater Error 0xffff0000 (-65536) -
2 - Panel A Finished processing Singlechip NAND <LIST/> : FAIL code=-65536.
Panel A: Operation stopped by user.
Please see why debug UART is not working:
- where is it connected (AUART0, I2C0 or PWM pins)?
- are fuses in i.MX28 burned accordingly (USE_ALT_DEBUG_UART_PINS)?
Already internal ROM should be printing out on that port so it's extremely useful for debugging. And it's much more informative than output from MfgTool itself.
Here is the debug print log :
PowerPrep start initialize power...
Configured for 5v only power source. Battery powered operation disabled.
LLLCOct 30 201217:58:53
FRAC 0x92925552
memory type is DDR2
Wait for ddr ready 1power 0x00820616
Frac 0x92925552
start change cpu freq
hbus 0x00000003
cpu 0x00010001
start test memory accress
ddr2 0x40000000
finish simple test
LLLLLLLFLCLFLLJUncompressing Linux... done, booting the kernel.
VEN--> init/main.c 541
Linux version 2.6.35.3-571-gcca29a0 (hari@MELANGE) (gcc version 4.4.4 (4.4.4_09.06.2010) ) #3 PREEMPT Wed Dec 12 14:59:53 IST 2012
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: Freescale MX28EVK board
Memory policy: ECC disabled, Data cache writeback
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512
Kernel command line: console=ttyAM0,115200 rdinit=/linuxrc rw gpmi
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 128MB = 128MB total
Memory: 119636k/119636k available, 11436k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xfde00000 - 0xffe00000 ( 32 MB)
vmalloc : 0xc8800000 - 0xf0000000 ( 632 MB)
lowmem : 0xc0000000 - 0xc8000000 ( 128 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc0046000 ( 248 kB)
.text : 0xc0046000 - 0xc056a000 (5264 kB)
.data : 0xc056a000 - 0xc05a5e40 ( 240 kB)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
RCU-based detection of stalled CPUs is disabled.
Verbose stalled-CPUs detection is disabled.
NR_IRQS:296
Console: colour dummy device 80x30
console [ttyAM0] enabled
Calibrating delay loop... 226.09 BogoMIPS (lpj=1130496)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux: Initializing.
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
regulator: core version 0.5
NET: Registered protocol family 16
regulator: vddd: 800 <--> 1575 mV at 1500 mV fast normal
regulator: vdddbo: 800 <--> 1575 mV fast normal
regulator: vdda: 1500 <--> 2275 mV at 1800 mV fast normal
vddio = 3380000, val=10
regulator: vddio: 2880 <--> 3680 mV at 3380 mV fast normal
regulator: overall_current: fast normal
regulator: vbus5v:
regulator: mxs-duart-1: fast normal
regulator: mxs-bl-1: fast normal
regulator: mxs-i2c-1: fast normal
regulator: mmc_ssp-1: fast normal
regulator: mmc_ssp-2: fast normal
regulator: charger-1: fast normal
regulator: power-test-1: fast normal
regulator: cpufreq-1: fast normal
i.MX IRAM pool: 124 KB@0xc8820000
Initializing GPMI pins
VEN--> arch/arm/mach-mx28/device.c 754 mx28_init_mmc MMC0 is enabled
usb DR wakeup device is registered
IMX usb wakeup probe
audit: cannot initialize inotify handle
bio: create slab <bio-0> at 0
GCD register_devices:371
EEPROM MISC is Register
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource mxs clock source
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (junk in compressed archive); looks like an initrd
Freeing initrd memory: 4096K
Bus freq driver module loaded
IMX usb wakeup probe
usb h1 wakeup device is registered
GCD drivers/gpio/pca953x.c:207:8
Probing at24_probe ..
page_size 16, num_addresses 4, write_max 16, use_smbus 0
at24 Reading ...
Done
mxs_cpu_init: cpufreq init finished
audit: initializing netlink socket (disabled)
type=2000 audit(0.750:1): initialized
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 4.0 (2009/01/31) Phillip Lougher
JFS: nTxBlock = 966, nTxLock = 7733
msgmni has been set to 241
alg: No test for stdrng (krng)
cryptodev: driver loaded.
Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
LVDS GPIO 21
GCD init_panel:80
lcdif_set_rate:1157
GCD: init_bl:246
GCD mxsbl_set_intensity:239
GCD set_bl_intensity:316: Intensity 50
GCD bl_to_power:298
GCD bl_to_power:298
SIVA: drivers/video/fbmem.c fb_prepare_logo 575
SIVA: drivers/video/fbmem.c fb_prepare_logo 593
SIVA: drivers/video/fbmem.c fb_prepare_logo 600
SIVA: drivers/video/fbmem.c fb_prepare_logo 636
Console: switching to colour frame buffer device 60x34
SIVA: drivers/video/fbmem.c fb_show_logo_line 434
SIVA: drivers/video/fbmem.c fb_show_logo_line 473
SIVA: drivers/video/fbmem.c fb_do_show_logo 398
GCD blank_panel:196
GCD release_panel:185
GCD free_bl:270
GCD init_panel:80
lcdif_set_rate:1157
GCD: init_bl:246
GCD mxsbl_set_intensity:239
GCD set_bl_intensity:316: Intensity 50
GCD bl_to_power:298
GCD bl_to_power:298
GCD blank_panel:196
IMX28 LRADC Temperature Driver Version 1 (C)
IMX28 LRADC Temperature Driver Version 1 (C) GCD
IMX28 LRADC Temperature Driver is Register with Minor number 1
mxs-duart.0: ttyAM0 at MMIO 0x80074000 (irq = 47) is a DebugUART
------------------ROHIT : recent ---------------
mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0
Found APPUART 3.1.0
------------------ROHIT : recent ---------------
mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 113) is a mxs-auart.1
Found APPUART 3.1.0
------------------ROHIT : recent ---------------
mxs-auart.2: ttySP2 at MMIO 0x8006e000 (irq = 114) is a mxs-auart.2
Found APPUART 3.1.0
------------------ROHIT : recent ---------------
mxs-auart.3: ttySP3 at MMIO 0x80070000 (irq = 115) is a mxs-auart.3
Found APPUART 3.1.0
------------------ROHIT : recent ---------------
mxs-auart.4: ttySP4 at MMIO 0x80072000 (irq = 116) is a mxs-auart.4
Found APPUART 3.1.0
brd: module loaded
loop: module loaded
Misc MDB Device driver
MISC MDBD Driver is registered
i.MX GPMI NFC
NFC: Version 1, 8-chip GPMI and BCH
Boot ROM: Version 1, Single-chip boot area, block mark swapping supported
Scanning for NAND Flash chips...
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xf1 (Micron NAND 128MiB 3,3V 8-bit)
mfr_id 2c
nand_device_mfr_directory[0].id: 98
nand_device_mfr_directory[1].id: ec
nand_device_mfr_directory[2].id: 4
nand_device_mfr_directory[3].id: 8f
nand_device_mfr_directory[4].id: 7
nand_device_mfr_directory[5].id: 20
nand_device_mfr_directory[6].id: ad
nand_device_mfr_directory[7].id: 2c
attempt identify device
-----------------------------
NAND Flash Device Information
-----------------------------
Manufacturer : Micron (0x2c)
Device Code : 0xf1
Cell Technology : SLC
Chip Size : 128 MiB
Pages per Block : 64
Page Geometry : 2048+64
ECC Strength : 4 bits
ECC Size : 512 B
Data Setup Time : 30 ns
Data Hold Time : 20 ns
Address Setup Time: 10 ns
GPMI Sample Delay : 6 ns
tREA : Unknown
tRLOH : Unknown
tRHOH : Unknown
Description : <None>
-----------------
Physical Geometry
-----------------
Chip Count : 1
Page Data Size in Bytes: 2048 (0x800)
Page OOB Size in Bytes : 64
Block Size in Bytes : 131072 (0x20000)
Block Size in Pages : 64 (0x40)
Chip Size in Bytes : 134217728 (0x8000000)
Chip Size in Pages : 65536 (0x10000)
Chip Size in Blocks : 1024 (0x400)
Medium Size in Bytes : 134217728 (0x8000000)
------------
NFC Geometry
------------
ECC Algorithm : BCH
ECC Strength : 8
Page Size in Bytes : 2112
Metadata Size in Bytes : 10
ECC Chunk Size in Bytes: 512
ECC Chunk Count : 4
Payload Size in Bytes : 2048
Auxiliary Size in Bytes: 16
Auxiliary Status Offset: 12
Block Mark Byte Offset : 1999
Block Mark Bit Offset : 0
-----------------
Boot ROM Geometry
-----------------
Boot Area Count : 1
Boot Area Size in Bytes : 20971520 (0x1400000)
Stride Size in Pages : 64
Search Area Stride Exponent: 2
Scanning device for bad blocks
Boot area protection is enabled.
uboot : c04f0c3d
u-boot env : 0
kern1 : 0 fs1 : 1e0000 kern2 : 0 fs2 : 200000 application : 0
Creating 7 MTD partitions on "gpmi-nfc-main":
0x000000000000-0x0000001e0000 : "u-boot"
0x0000001e0000-0x000000200000 : "u-boot-env"
0x000000200000-0x000000700000 : "kern1"
0x000000700000-0x000002f00000 : "fs1"
0x000002f00000-0x000003400000 : "kern2"
0x000003400000-0x000005c00000 : "fs2"
0x000005c00000-0x000008000000 : "gpmi-nfc-general-use"
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
usbcore: registered new interface driver asix
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver MOSCHIP usb-ethernet driver
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
GCD blank_panel:196
GCD blank_panel:196
GCD blank_panel:196
GCD blank_panel:196
fsl-ehci fsl-ehci: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci: irq 93, io base 0x80080000
fsl-ehci fsl-ehci: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: Freescale On-Chip EHCI Host Controller
usb usb1: Manufacturer: Linux 2.6.35.3-571-gcca29a0 ehci_hcd
usb usb1: SerialNumber: fsl-ehci
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
can't find transceiver
fsl-ehci fsl-ehci: init fsl-ehci fail, -19
GCD blank_panel:196
GCD blank_panel:196
GCD blank_panel:196
GCD blank_panel:196
GCD blank_panel:196
GCD blank_panel:196
GCD blank_panel:196
GCD blank_panel:196
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.0: irq 92, io base 0x80090000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: Freescale On-Chip EHCI Host Controller
usb usb2: Manufacturer: Linux 2.6.35.3-571-gcca29a0 ehci_hcd
usb usb2: SerialNumber: fsl-ehci.0
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
usbcore: registered new interface driver cdc_acm
cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbserial
usbserial: USB Serial Driver core
USB Serial support registered for Sierra USB modem
usbcore: registered new interface driver sierra
sierra: v.1.7.16:USB Driver for Sierra Wireless USB modems
ARC USBOTG Device Controller driver (1 August 2005)
Can't find OTG driver!
mice: PS/2 mouse device common for all mice
input: MXS touchscreen as /devices/virtual/input/input0
rtc-pcf8563 1-0051: chip found, driver version 0.4.3
rtc-pcf8563 1-0051: rtc core: registered rtc-pcf8563 as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
mxs-pxp mxs-pxp.0: initialized
mxs watchdog: initialized, heartbeat 19 sec
mxs-mmc: MXS SSP Controller MMC Interface driver
__mxs_reset_block(f0010000): timeout when resetting
mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 82 ERRIRQ 96
dcp dcp.0: DCP crypto enabled.!
usbcore: registered new interface driver snd-usb-audio
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
rtc-pcf8563 1-0051: low voltage detected, date/time is not reliable.
rtc-pcf8563 1-0051: setting system clock to 2000-04-11 06:00:39 UTC (955432839)
RAMDISK: Couldn't find valid RAM disk image starting at 0.
Root-NFS: No NFS server available, giving up.
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "(null)" or unknown-block(2,0)
Please append a correct "root=" boot option; here are the available partitions:
1f00 1920 mtdblock0 (driver?)
1f01 128 mtdblock1 (driver?)
1f02 5120 mtdblock2 (driver?)
1f03 40960 mtdblock3 (driver?)
1f04 5120 mtdblock4 (driver?)
1f05 40960 mtdblock5 (driver?)
1f06 36864 mtdblock6 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
Backtrace:
[<c004a60c>] (dump_backtrace+0x0/0x114) from [<c0431af0>] (dump_stack+0x18/0x1c)
r7:c04ec77d r6:00008000 r5:c77f1000 r4:c05a6d28
[<c0431ad8>] (dump_stack+0x0/0x1c) from [<c0431b6c>] (panic+0x78/0xf4)
[<c0431af4>] (panic+0x0/0xf4) from [<c0009048>] (mount_block_root+0x1d8/0x218)
r3:00000000 r2:00000001 r1:c7c27f60 r0:c04ec824
[<c0008e70>] (mount_block_root+0x0/0x218) from [<c000914c>] (mount_root+0xc4/0xfc)
[<c0009088>] (mount_root+0x0/0xfc) from [<c00092f0>] (prepare_namespace+0x16c/0x1d0)
r5:c002a4c8 r4:c05a6100
[<c0009184>] (prepare_namespace+0x0/0x1d0) from [<c00084f8>] (kernel_init+0x128/0x174)
r5:c002a4c8 r4:c05a5ec0
[<c00083d0>] (kernel_init+0x0/0x174) from [<c0068aac>] (do_exit+0x0/0x750)
r5:c00083d0 r4:00000000
...looks like my kernel configuration in LTIB is different then which is required to program NAND. Thanks.
What are you booting here - updater firmware kernel on your custom board, or is this "full" Linux kernel you'd like to boot on your custom board?
In any case, kernel is not able to find root partition to mount. Where is it stored?
In case this is updater firmware, there should be initramfs stored after the linux kernel.
In case this is full kernel, you should pass a "root=" parameter to kernel to tell it where to locate file system on (NAND, SD, NFS...).
Thanks for reply Vladan, It is updater firmware..and if you check log for custom Board, in line no. 99 and 100 you will see:
"
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (junk in compressed archive); looks like an initrd
" ... I don't understand why is it saying that because this initramfs is generated from a LTIB option only..Any idea.
Not sure either. Did you generate updater binary from a separate LTIB installation or from the same one where you build your normal Linux environment?
From what I know updater binary should be built from separate install, as then you choose Manufacturing firmware profile very early during one of first LTIB setup screen. It won't work otherwise I believe.