i.MX28 SSP_SCK Polarity issue: Provided patch not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 SSP_SCK Polarity issue: Provided patch not working

1,898 Views
katte
Contributor II

Hi, I'm in trouble with the "boot from sd" issue.

I have a board that boot from ssp0 sd card. Fortunately I've a eeprom in my pcb.

I've programmed the eeprom with the freescale provided patch:

Patch for the SDK 2010.12 to fix the incorrect polarity when boot mode is set as boot from SD/eMMC o...

but the boot still fail when try to mount root fs.

No filesystem could mount root, tried:  ext3 ext2 vfat msdos iso9660 ntfs

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)

Backtrace:

[<c00344a8>] (dump_backtrace+0x0/0x114) from [<c03f1330>] (dump_stack+0x18/0x1c)

r7:c04a59ae r6:00008000 r5:c7c16022 r4:c05663d8

[<c03f1318>] (dump_stack+0x0/0x1c) from [<c03f13ac>] (panic+0x78/0xf4)

[<c03f1334>] (panic+0x0/0xf4) from [<c000902c>] (mount_block_root+0x1d8/0x218)

r3:00000000 r2:00000020 r1:c7c27f60 r0:c04a5a55

[<c0008e54>] (mount_block_root+0x0/0x218) from [<c0009130>] (mount_root+0xc4/0xf         c)

[<c000906c>] (mount_root+0x0/0xfc) from [<c00092d4>] (prepare_namespace+0x16c/0x         1c4)

r5:c0029a29 r4:c0565760

[<c0009168>] (prepare_namespace+0x0/0x1c4) from [<c00084f8>] (kernel_init+0x128/         0x170)

r5:c0028bd8 r4:c0565520

[<c00083d0>] (kernel_init+0x0/0x170) from [<c005010c>] (do_exit+0x0/0x6dc)

r5:c00083d0 r4:00000000

Obviously the sd and the root fs is ok, I've already done all the hardware controls and I'm sure is all right. I'm sure that the boot is from eeprom, because I've controlled it with an oscilloscope.

I've found only a solution, if I make a reset after the kernel panic, the board reboots itself and the boot process is ok.

Anyone have a solution that works for this incredibly (no fix scheduled) problem?

Thanks to all in advance.

Labels (2)
0 Kudos
10 Replies

1,001 Views
alamandachandra84
Contributor I

Hi,

 

We are having issue with SD card and want to try the patch, mentioned in this thread. I am trying to access L2.6.35_10.12_SSP_CLK_PATCH_UP patch file specified in the link Patch for the SDK 2010.12 to fix the incorrect polarity when boot mode is set as boot from SD/eMMC o...and it is opening a blank page. I am not sure, if this patch is available are not.

 

Can you please provide the link or reshare it. 

 

Best regards,

Poorna Chandra Sekhar.

0 Kudos

1,405 Views
jimmychan
NXP TechSupport
NXP TechSupport

which version of BSP or kernel are you using? Have you try the latest BSP?

what type of your rootfs? ext3 or ext4 will be more stable.

have you try different SD cards?

0 Kudos

1,405 Views
katte
Contributor II

I use LTIB 2.6.35_10.12.01 BSP, my rootfs is formatted in ext3.

I tried several sd cards on my board and on EVK.

I've used kingston, verbatim and samsung micro sd card class 4. And also a team micro sd card class 10.

I'am waiting some industrial micro sd cards for other tests.

Some sd cards have problems on some of my board but not on others.

The same sd cards sometimes works without problem on the EVK, sometimes not.

I've noted that sd cards class 10 seems to work better.

The kernel is always loaded without problem, Only when it load the rootfs the kernel panic appear.

I've also tried with and without the boot from eeprom, but the result is the same.

When the system start, I'm able to execute my program without any error. My program fill the 80% of the ram present in the board. That's why I think my ram is ok.

What I don't understand is this.

If my board goes to panic, if I made a reset, the board reboot itself and the next boot is always ok.

Another thing that i don't understand is this.

The patch tell me that the problem is in clock polarity at startup.

""When boot mode is set as boot from SD/eMMC on SSP0/1, the SSP_SCK polarity is not correctly setup in ROM. The POLARITY bit in HW_SSP_CTRL1 register should be set to “1” – command and data output on falling edge of clock – according to SD and eMMC specification. However the POLARITY bit is set to “0” in ROM in existing silicon (TO1.2). As a result, input setup time (tISU) at SD/eMMC input may not be met.""

Ok, but why this affects the mount of the rootfs? The linux kernel don't set this register correctly?

Thanks in advance.

Regards.

0 Kudos

1,405 Views
jimmychan
NXP TechSupport
NXP TechSupport

Did you apply the patches for 10.12?

There is a newer version of BSP, you may try to use the newer version (L2.6.35_1.1.1) .

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&fpsp=1&tab=Design_Tools_T...

1,405 Views
katte
Contributor II

Yes, I've applied all the patches.

I'm downloading the new bsp now. I will try it immediately.

Thanks in advance.

0 Kudos

1,405 Views
katte
Contributor II

I'm trying the demo kernel and it seems to work perfectly on 3 different sd cards.

Now I will try to recompile the kernel with ltib and retest the system.

Thanks for the hint!

0 Kudos

1,405 Views
igorpadykov
NXP Employee
NXP Employee

I think that patch has not relation to rootfs problem.

These may be signal inegrity issues, so recommended to check

signals by oscilloscope. These may be brownout issues,

due to ripples o power supplies lines.

One can try to test SD transfers with OBDS test

host_data_write,read (mx28_sd.c)

"IMX_OBDS  : On-Board Diagnostic Suit for the i.MX28"

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&fpsp=1&tab=Design_Tools_T...

~igor

0 Kudos

1,405 Views
katte
Contributor II

As I expected.

I referred to this patch because in the past I had asked to a freescale FAE, and he told me to try this patch.

Thanks for your help.

Now I'm trying to run the obd tests.

In the pdf attached there is a link for get Sourcery G++ Lite 2008q3-66 (http://compass.freescale.net/go/217844329), but this link isn't working.

Do you know where I can find this program?

There is a chance to compile obd with the tools included in ltib?

Another question, do you know how to debug linux kernel directly on the board with jtag? I have the  keil ulink pro jtag probe.

0 Kudos

1,405 Views
igorpadykov
NXP Employee
NXP Employee

Hi Marco

I think you can easily port obds (just one sd test) to keil,

it is not big size. Regarding debug it may be useful to check

http://cache.freescale.com/files/32bit/doc/app_note/AN4553.pdf

Best regards

igor

0 Kudos

1,405 Views
igorpadykov
NXP Employee
NXP Employee

Hi Marco

had you updated DDR settings with tool below

Board Bring-up and DDR Initialization Tools

also, had you tried other SD cards and does this SD boot

with i.MX28EVK ?

Best regards

igor

0 Kudos