i.MX28 SAIF pins state in running and standby mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX28 SAIF pins state in running and standby mode

855件の閲覧回数
jörgkrause
Contributor I


Hi,

I have a question and an issue with the i.MX28 SAIF pins using the Mainline kernel version 4.7.

Why is the MCLK always active, even if no audio playback is started?

If the CPU goes into standby mode, the output state of the MCLK and BITCLK are not reliable. Sometimes they go into HIGH state, another time into LOW state. What is the supposed behavior for these pins in standby mode?

Jörg Krause

EDIT: Note about Mainline kernel and version.

ラベル(2)
0 件の賞賛
1 返信

655件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Joerg

as answered on below link nxp does not support kernel mainline.

kobs-ng with 4.4+ kernels on imx6 processors

One can test with latest bsp from product page and port necessary changes

Board Support Packages (4)

i.MX28 Linux 2.6.35 Source Code Files and documentation (REV L2.6.35_1.1.0)

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛