i.MX28 On-Board Diagnostics Suite (OBDS)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 On-Board Diagnostics Suite (OBDS)

2,428 Views
IvanRia
Contributor II

hello everyone, I need a full memory check for the imx28 system, I met a mention of this utility: i.MX28 On-Board Diagnostics Suite (OBDS), but did not find where it can be downloaded, please tell me where it can be downloaded? also wondering if this utility can do a full memory check?

0 Kudos
Reply
5 Replies

2,424 Views
IvanRia
Contributor II

i found this. the second question is relevant, is it possible to check all memory

0 Kudos
Reply

2,421 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply

2,418 Views
IvanRia
Contributor II

Thank you, Yuri, I looked at On-Board Diagnostic Suit for the i.MX28, however I found the following lines in the pdf file: "This test should not be confused with a stress test that validates robust signal integrity of the interface."

but I need a stress test for the whole RAM, tell me if there is such a tool for the imx28 system?

0 Kudos
Reply

2,409 Views
Yuri
NXP Employee
NXP Employee

I've sent You some comments directly.

~Yuri. 

0 Kudos
Reply

2,421 Views
IvanRia
Contributor II

another question, is there a memory test for the imx28 system similar to this one: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-6-7-DDR-Stress-Test-Tool/ta-p/11082...

0 Kudos
Reply