What read/write speeds should I expect from the i.MX28 NAND?
I'm only seeing between 1-2MB/sec which seems very slow. Read/write speeds from/to SD Card are quite a bit faster.
I've tried bumping up the GPMI clock from the default 24MHz to 48MHz and higher. The max speed increase was around 10%. This was with kernel version 4.10 and 4.19.
I'm using two S34ML08G1 NAND devices.
Hi Manuel
one can check below link (attachments were sent via mail)
Adding Support For a New NAND with i.MX28–NAND Analysis
On i.MX28 EVK with K9LBG08U0D there were 2-3MB/s results.
https://community.nxp.com/message/311702#311702
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------