i.MX28 NAND CRC failed at low temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 NAND CRC failed at low temperature

Jump to solution
1,133 Views
torus1000
Contributor V

Hi,

I tested NAND boot for our iMX283 product at low temperature then boot failed about 1/80 set.
Error code was "0x8050100b" which means "Load command payload CRC failed".
Is there anyone can help?

(Q) Does it mean CRC of read data during LDR instruction period failed? Why this fail happen?

(Q) Which part of i.MX28 detect CRC fail? BCH hardware or software?

(Q) How can I avoid this CRC fail?

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
807 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

error message 0x8050100b may mean presence of

NAND bad block. It may be recommended update NAND timings

and rewrite NAND with flash_eraseall,  kobs-ng , e.t.c.

Adding Support For a New NAND with i.MX28–NAND Analysis

Also this may be related to this particular NAND part

(it may be weared out), so one can try fresh new NAND.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
808 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

error message 0x8050100b may mean presence of

NAND bad block. It may be recommended update NAND timings

and rewrite NAND with flash_eraseall,  kobs-ng , e.t.c.

Adding Support For a New NAND with i.MX28–NAND Analysis

Also this may be related to this particular NAND part

(it may be weared out), so one can try fresh new NAND.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply