i.MX28 : L2.6.35_10.12_SSP_CLK_PATCH_UP patch with VDD5V Source Only

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 : L2.6.35_10.12_SSP_CLK_PATCH_UP patch with VDD5V Source Only

Jump to solution
633 Views
koichisakagami
Contributor II

Dear community,
I have a question about L2.6.35_10.12_SSP_CLK_PATCH_UP patch modification.

[Background]
For TKT131240 errata ( SSP_SCK polarity setup issue in ROM ) ,
I have to use a L2.6.35_10.12_SSP_CLK_PATCH_UP patch.

And I would like to use VDD5V Source Only (AN4199 section 4.1.2.1) implementation .

[Question]
In order to work correctly with VDD5V Source Only,
how should I modify the patch file ?

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
1 Solution
473 Views
Yuri
NXP Employee
NXP Employee

It is need to use the patch for VDD5V configuration too.


Have a great day,
Yuri
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
474 Views
Yuri
NXP Employee
NXP Employee

It is need to use the patch for VDD5V configuration too.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos