Hello,
How to burn Operating system to NAND Flash along with bootlader in i.MX28 EVK. Can we do it directly from MMC using commands or do we need to use the USB OTG?
Solved! Go to Solution.
Please refer to section 5.1.3.2 (NAND Boot) of "MX28_EVK_Linux_User_Guide.pdf".
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Sure, you can do that via MMC. Just you have to make sure that kernel has support for NAND flash.
It can be done using:
1) Boot via u-boot and flash rootfs to NAND
2) Boot via Linux on MMC and flash rootfs to NAND.
In both cases, you need to update the u-boot parameters n there you go..Good Luck!!
Thanks Ankur for the info can you explain how these two steps can be done. Is the any document or tutorial available?
Please refer to section 5.1.3.2 (NAND Boot) of "MX28_EVK_Linux_User_Guide.pdf".
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------