i.MX28 EMAC and IP accelerator functions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX28 EMAC and IP accelerator functions

877件の閲覧回数
stathisv
Contributor II

Hi all,

I am trying to enable IP header checksum insertion by the EMAC on the transmit path.

Although I set bit 3 (TX_IPCHK_INS) of register HW_ENET_MAC_IPACCTXCONF it does

not seem to have any effect. When I capture the packet with Wireshark the checksum

is still 0. Does this feature work in the legacy DMA mode?

I noticed that in the enhanced DMA mode this feature can be enabled via a control bit

on the DMA descriptor too.

Regards,

Stathis

ラベル(1)
0 件の賞賛
返信
0 返答(返信)