i.MX28 283 Battery Charger :: How to Force charger ON (for Li-Ion cell)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 283 Battery Charger :: How to Force charger ON (for Li-Ion cell)

984 Views
bempey
Contributor I

We've been designing products for > 5 years with the iMX28, and have many thousands deployed in harsh environments on multiple continents (and off-shore) with great success.

But recently, we've started using the battery as  a means to avoid brown-out issues. (more specifically, cold-cranking voltage drop-outs)

The battery works great ... when it works.

However, we have an issue with new systems with un-charged batteries.

We're using  a raw single Li-Ion cell, with the (Seiko) protection chip on our board.

As you know, the protection chips cut-off current below 2 volts.

We have a resistor in parallel with the chip to allow a fresh board to be trickle-charged till the battery voltage comes up safely to a level for normal charging.

SYMPTOM
When powering up a fresh (new) system with an uncharged battery, the charger is not turned on.

ISSUE

The protection circuit adds a high-impedance between the battery and GND, causing the battery-detection circuit to fail.
If the unit is power-cycled after the battery is charged, then its OK.  Trouble is, our systems are buried in heavy trucks, operating 24/7 with union drivers, and they're hard-wired to the battery to run always, forever (the Ignition signal is an Input we monitor, not a power source). You can't say "just go disconnect the battery for a minute and re-connect".  To power-cycle the unit, it must be booked into a service facility.  Not easy. Not cheap.

PROBLEM 

We need to force the charger ON regardless of whether it detects the battery or not.

BETS

I bet its just flipping one bit.

HOPES

I hope there's a library of run-time battery management utilities that includes such things as battery control, reading the battery voltage, etc.

(We're fine with the startup configurations, and setting the charge current limits and charge threshold.)

But I've been searching for days and can't find it/one.

DISCLAIMER

I wrote SW for 3 decades, but never advanced to Linux programming.

I'm posting this on behalf of my lead system programmer.

I hope the information is clear enough.

THANKS!

Labels (1)
0 Kudos
Reply
2 Replies

728 Views
bempey
Contributor I

Thanks Artur!

Sorry for the delay. HD packed it in on my laptop. Its not back up and running, with a 1/4 TB SSD for Linux Mint & Win7, and a 1 TB Hydrid drive for data files.

We're going to try that.

Still can't find any source-code anywhere that implements proper battery-handling for portable devices.

0 Kudos
Reply

728 Views
art
NXP Employee
NXP Employee

You have to clear the PWD_BATTCHRG bit in the HW_POWER_CHARGE register to switch the battery charging circuit on. For more information, please refer to the i.MX28 Reference Manual document.

For the information on the Linux driver for the i.MX28 power supply and battery charger circuit, please refer to the Chapter 27 of the latest i.MX28 EVK Linux Refernce Manual document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply