i.MX27 High Speed USB and charging paths.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX27 High Speed USB and charging paths.

742件の閲覧回数
ime95mos
Contributor I

I am using a i.MX27L together with the MC13783 chip.

 

I am not using the builtin USB Full speed circuit in MC13783, instead I have added a High Speed PHY from SMSC with OTG Support on the OTG port.

 

Currently I have a seperate dual path configuration for the power supply. How can I charge from both a USB Host (PC) and Wall adapter without pulling more than 500mA from the USB Host? Can it be solved by changing the path or do I need externa circuits ?

タグ(2)
0 件の賞賛
返信
0 返答(返信)