i.MX27 Adjusting the 26 MHz Oscillator Trim when using an oscillator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX27 Adjusting the 26 MHz Oscillator Trim when using an oscillator

512件の閲覧回数
craighillis
Contributor I

When using an external oscillator as the 26MHz source, we can not adjust the amplitude to the desired range based on section 3.4.8.1 Adjusting the 26 MHz Oscillator Trim of the reference manual. I have tried reducing the drive voltage from the oscillator but it did not help. the OSC26M_AGC[5:0] register is 0 and the OSC26M_PEAK[1:0] says I need to trim lower.

We do not have this problem when using a 26MHz crystal.

When using the external oscillator, we can not properly shutdown the MPLL to go to low power sleep.

Could the sleep problem with the external oscillator have anything to do with the trim adjustment problem?

0 件の賞賛
返信
1 返信

444件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  is it possible to look at the scheme ?

You may create request to provide the design scheme :

How to submit a new question for NXP Support

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信