i.MX27 Adjusting the 26 MHz Oscillator Trim when using an oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX27 Adjusting the 26 MHz Oscillator Trim when using an oscillator

792 Views
craighillis
Contributor I

When using an external oscillator as the 26MHz source, we can not adjust the amplitude to the desired range based on section 3.4.8.1 Adjusting the 26 MHz Oscillator Trim of the reference manual. I have tried reducing the drive voltage from the oscillator but it did not help. the OSC26M_AGC[5:0] register is 0 and the OSC26M_PEAK[1:0] says I need to trim lower.

We do not have this problem when using a 26MHz crystal.

When using the external oscillator, we can not properly shutdown the MPLL to go to low power sleep.

Could the sleep problem with the external oscillator have anything to do with the trim adjustment problem?

0 Kudos
Reply
1 Reply

724 Views
Yuri
NXP Employee
NXP Employee

Hello,

  is it possible to look at the scheme ?

You may create request to provide the design scheme :

How to submit a new question for NXP Support

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply