i.MX25x and i.MX25PDK - wall comments

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX25x and i.MX25PDK - wall comments

896 Views
Frias
Contributor V
For developers working with i.MX25x and its development tool, the i.MX25PDK.
Labels (1)
0 Kudos
Reply
3 Replies

680 Views
MehmetAliIpin
Contributor V

Hello dear group members,

We have a POS project with i.mx 258. We have prepared a prototype for the main processor, memory and various IO modules. We also have i.mx25PDK kit.

I have built a working NFS for the kit and ubuntu 10.10. 

I am glad, there is a group for the i.mx25 and its pdk.

With my best wishes

0 Kudos
Reply

680 Views
x10
Contributor V
I try to use MfgTool to program iMX25 with NandFlash. Where can I get find an ucl.xml. Thanks!
0 Kudos
Reply

680 Views
Oceanblue
Contributor III

Dear all,      

      YUANYING Tech has invested a lot of resource in the system design with FREESCALE ARM series product, up to date we have launched the series development platform based on i.MX28、i.MX35、i.MX51,largely help our customers shorten the time to market about their product and create the success one and another. Now we are proud to announce we have launched i.MX25 Linux system level platform:YY-i.MX25L。

 

    i.MX25L is the system platform based on Linux 2.6.31 kernel,treat ext2 as system file,  own i.mx258+128MB DDR2 system hardware, be able to boot up form SD card or NAND Flash,also i.MX25L including 7” LCD and resistance touch panel. Which built in i.MX25 all input/output resource. Which still adopt core board + bottom board structure,the components of CPU core board meet the industrial level,be able to work at the temperature range of -40C to +85C,and storage temperature from  -55C to +125 degree. i.MX25L can widely applied for intelligent electric network, outdoor multimedia, industrial control and HMI, medical equipment and so on .Which is the good selection to power meter terminal, HMI of industry equipment, automotive ECU, medical device display interface。

    About the business model, YUANYING support core board selling and PCBA business model. And, promise to deliver the cost effective performance among ARM9 system to her customers.

 

     Visiting www.yuan-ying.com for the detail.

 

     62-IMG_0002sysBoard.jpg

64-image001Linux.jpg

0 Kudos
Reply