Yes thanks, but we use this configuration :
Hardware PIN configuration :
- BT_DPARE_SIZE = 218
- BT_MLC-SEL = SLC
- BT_PAGE_SIZE = 2k
- BT_MEM_CTRL = Nand Flash
- BT_MEM_TYPE = 5 address cycles
After a power on, we can read 0x640001E0 value in the RCSR regsiter.
For us, it seems correct.
We are checking the NFC controler configuration...
In NAND_FLASH_CONFIG1 register (0xBB001E1A), we can read 0x0C0A. It seems not correct,
If we set 0x0A09 in this register using our hardware debug probe (by using a breakpoint just after the reading of RCSR register) => barebox starts well.
If is set the same configuration in the DCD table (inside our barebox binary file) : it doesn't work.
Maybe DCD configuration is applied too late...
Is it possible to configure or (re-configure) the NFC controler with the DCD table?
Loic