i.MX25 IOMUXC_SW_PAD_CTL_PAD_D08-1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX25 IOMUXC_SW_PAD_CTL_PAD_D08-1

631 Views
norishinozaki
Contributor V

Hello Champs,

In i.MX25,  IOMUXC_SW_PAD_CTL_PAD_D15 - D08 can be set PKE, PUE, PUS, etc as follows.

pastedImage_1.png

However for IOMUXC_SW_PAD_CTL_PAD_D07 - D1,  only PUE can be set as followpastedImage_0.png

Does the "1: Pull mean" mean "Pullup" correct?

Then what is the Ω inside,

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
Reply
2 Replies

395 Views
Yuri
NXP Employee
NXP Employee

Hello,

shortly - 100 KOM pullup.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

395 Views
norishinozaki
Contributor V

Hello Yuri,

Thank you!

Nori Shinozaki

0 Kudos
Reply