I have some questions about the i.MX233 package variants:
1. Is it possible to identify the the package variant (LQFP128, BGA169) of the i.MX233 via register?
2. How should be HW_CLKCTRL_ETM and HW_CLKCTRL_PIX treat on LQFP128?
解決済! 解決策の投稿を見る。
you are right, sorry I missed that:
HW_DIGCTL_STATUS[PACKAGE_TYPE]: package type. 000=169BGA, 011=128TQFP
Table 6-4. HW_DIGCTL_STATUS i.MX23 Reference Manual (rev.1, 11/2009).
http://www.freescale.com/files/dsp/doc/ref_manual/IMX23RM.pdf
Best regards
igor
Now i'm a little bit confused. According to i.MX23 reference manual chapter 6.4.2 there should be a register to identify the package variant (HW_DIGCTL_STATUS_PACKAGE_TYPE, 0=BGA, 3=LQFP), which is also in the bootlet code.
you are right, sorry I missed that:
HW_DIGCTL_STATUS[PACKAGE_TYPE]: package type. 000=169BGA, 011=128TQFP
Table 6-4. HW_DIGCTL_STATUS i.MX23 Reference Manual (rev.1, 11/2009).
http://www.freescale.com/files/dsp/doc/ref_manual/IMX23RM.pdf
Best regards
igor
Hi Stefan
1. no
2. HW_CLKCTRL_ETM can be considered as reserved,
HW_CLKCTRL_PIX is functional, since LQFP128 supports
ITU-R BT.656 8-bit+clock mode according to Table 1-1. i.MX23
Functions by Package i.MX23 RM.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------