i.MX233 package variants

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX233 package variants

Jump to solution
1,005 Views
lategoodbye
Senior Contributor I

I have some questions about the i.MX233 package variants:

1. Is it possible to identify the the package variant (LQFP128, BGA169) of the i.MX233 via register?

2. How should be HW_CLKCTRL_ETM and HW_CLKCTRL_PIX treat on LQFP128?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
846 Views
igorpadykov
NXP Employee
NXP Employee

you are right, sorry I missed that:

HW_DIGCTL_STATUS[PACKAGE_TYPE]:  package type. 000=169BGA, 011=128TQFP

Table 6-4. HW_DIGCTL_STATUS i.MX23 Reference Manual (rev.1, 11/2009).

http://www.freescale.com/files/dsp/doc/ref_manual/IMX23RM.pdf

Best regards

igor

View solution in original post

0 Kudos
Reply
3 Replies
846 Views
lategoodbye
Senior Contributor I

Now i'm a little bit confused. According to i.MX23 reference manual chapter 6.4.2 there should be a register to identify the package variant (HW_DIGCTL_STATUS_PACKAGE_TYPE, 0=BGA, 3=LQFP), which is also in the bootlet code.

0 Kudos
Reply
847 Views
igorpadykov
NXP Employee
NXP Employee

you are right, sorry I missed that:

HW_DIGCTL_STATUS[PACKAGE_TYPE]:  package type. 000=169BGA, 011=128TQFP

Table 6-4. HW_DIGCTL_STATUS i.MX23 Reference Manual (rev.1, 11/2009).

http://www.freescale.com/files/dsp/doc/ref_manual/IMX23RM.pdf

Best regards

igor

0 Kudos
Reply
846 Views
igorpadykov
NXP Employee
NXP Employee

Hi Stefan

1. no

2. HW_CLKCTRL_ETM can be considered as reserved,

HW_CLKCTRL_PIX is functional, since LQFP128 supports

ITU-R BT.656 8-bit+clock mode according to Table 1-1. i.MX23

Functions by Package  i.MX23 RM.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------