i.MX233 and SDIO multiplex

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX233 and SDIO multiplex

跳至解决方案
2,467 次查看
daveshah
Contributor I

Would it be possible to have both an SDIO wireless device and an SDHC card on one SSP of the i.MX233, using a multiplexer like TS3A27518E-Q1 or MAX4996? Also, could you do it simply by connecting the data lines together for the two cards and having separate CMD lines for each device?

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,041 次查看
JackyAtFreescal
Senior Contributor II

Quote from "SD Specifications Part 1 Physical Layer Specification Version 2.00"

3.5 Bus Topology

...

Common bus signals for multiple card slots are not recommended. A single SD bus should

connect a single SD card.

...

Regards,

Jacky

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,041 次查看
YixingKong
Senior Contributor IV

Hi David, did Jacky's answer helps you. If yes, please mark it as Correct Answer.

0 项奖励
回复
2,042 次查看
JackyAtFreescal
Senior Contributor II

Quote from "SD Specifications Part 1 Physical Layer Specification Version 2.00"

3.5 Bus Topology

...

Common bus signals for multiple card slots are not recommended. A single SD bus should

connect a single SD card.

...

Regards,

Jacky

0 项奖励
回复