i.MX233 - accessing GPIO within a C program

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX233 - accessing GPIO within a C program

946 次查看
ScottKerstein
Contributor III

Using an i.MX233 in 128 pin QFP Package and running a GNU/Linux (kernel 3.12.0 at the moment)


Would like to be able to access GPIO directly from within a C program.  Looked at the table 37-3 Pin-Multiplex for 128-Pin QFP within i.MX233 Product Data sheet (IMX23RM Rev.1 11/2009) and following pages.

Where would I be able to find the actual addresses rather than register descriptions?

Thanks in advance,

Scott


标签 (2)
1 回复

826 次查看
lydia_ziegler
NXP Employee
NXP Employee

Hi Scott,

Take a look at Appendix B (RM Rev 1) and see if this will answer the question.

Thanks,

Lydia