i.MX233 BGA boot after 20 second delay

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX233 BGA boot after 20 second delay

708 Views
PramodKumar
Contributor IV

Hi,

We are facing one problem in our i.MX233 BGA based board that it boot after 20 second delay after 0x8020a01d message then start the kernel , while same kernel boot immediate in i.MX233 (LQFP 128) board.

The debug boot sequence is given below:

 

HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFC

PowerPrep start initialize power...

Battery Voltage = 0.78V

No battery or bad batterydetected!!!.Disabling batteryvoltage measurements./r/nLLCAug 22 201215:25:39

EMI_CTRL 0x1C084040

FRAC 0x92926192

init_ddr_mt46v32m16_133Mhz

power 0x00820710

Frac 0x92926192

start change cpu freq

hbus 0x00000003

cpu 0x00010001

LLLLLLLFCLJUncompressing Linux... done, booting the kernel.



Labels (1)
0 Kudos
5 Replies

504 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pramod

what is full marking of i.MX233 BGA ?


Best regards

igor

0 Kudos

504 Views
PramodKumar
Contributor IV

Hi Igor,

The full marking is MCIMX233DJM4D A4 M88S

Regards,

Pramod

0 Kudos

504 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pramod

I could not find such part available for purchasing

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX233&cof=0&am=0&tab=Buy_Parametric...

Best regards

igor

0 Kudos

504 Views
PramodKumar
Contributor IV

Hi Igor,

The marking is B not D the complete marking is MCIMX233DJM4B A4 M88S.

Regards,

Pramod Kumar

0 Kudos

504 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pramod

for "B" part 0x8020a01d message is due to erratum

IMX23CE

0x8020A01D means ERROR_DDI_SD_MBR_NOT_FOUND

This  2229 erratum is fixed in new Rev.C silicon,  last letter "C" marking.

There is workaround (patch)

"IMX23 SD ROM PATCH: EEPROM Patch Workaround for Errata #2229"

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX233&fpsp=1&tab=Design_Tools_Tab

Best regards

igor

0 Kudos