i.MX pins tool output, usage in u-boot port?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX pins tool output, usage in u-boot port?

991 Views
richardhaydon
Contributor I

I have a custom i.MX6s based board, the pinning is described by a mex file.

Using the Pins for i.MX tool we can export dtsi, csv and iomux_config_core1.h files.

We need a port of uboot or barebox for the board, for which we will need a .cfg file including the DCD setup.

After much looking around I don't see how to use the pin tool output for that purpose.

Any pointers please?

Labels (2)
0 Kudos
Reply
1 Reply

871 Views
igorpadykov
NXP Employee
NXP Employee

Hi Richard

.cfg file including DCD updated manually using results from DDR test

https://community.freescale.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply