i.MX / i.MX RT DCP security module compatibility

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX / i.MX RT DCP security module compatibility

跳至解决方案
502 次查看
FMA
Contributor III

Hello,

I am currently implementing a new product using the MIMXRT1061 device using a uClinux BSP from Emcraft. I would like to make use of the DCP security module and have found that there is a linux driver (mxs-dcp) posted into the linux kernel that makes use of the DCP for i.MX25 / i.MX28 and i.MX6SL and i.MX6ULL devices.

According to what I have gathered, the DCP module of the i.MX RT1061 chip seems to work accordingly to what I have seen into the code.

(here is the kernel reference of the driver code I mention:

https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git/tree/drivers/crypto/mxs-dcp.c?id=...)

Can anybody tell me whether there is any specific difference in the i.MX RT 1061 instance of the DCP in comparison to the other above mentioned chips I should be aware of in my attempt to use this driver code for my target?

 

Thanks in advance.

0 项奖励
回复
1 解答
488 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
No, the IP of DCP is same for i.MX25 / i.MX28, i.MX6SL, i.MX6ULL and RT1061 devices.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
489 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
No, the IP of DCP is same for i.MX25 / i.MX28, i.MX6SL, i.MX6ULL and RT1061 devices.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复