[i.MX Yocto] Virtual Display X11 RDP for i.MX91

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[i.MX Yocto] Virtual Display X11 RDP for i.MX91

448件の閲覧回数
Zk47T
Contributor II

Hi all,

I’d like to double-check my understanding about display support on i.MX91 (FRDM board).

  • From what I can tell, the i.MX91 FRDM has no HDMI or MIPI-DSI (or other display) outputs on the board, and I’m not seeing a display controller exposed by the SoC in the BSP.

  • My goal was to run a lightweight GUI remotely just for testing Yocto apps.

What I tried

  • Built core-image-sato (X11) and set up xrdp. The RDP session connects, but I only get a terminal session (no Sato desktop).

63eaadc99173192d4062.jpg

  • Doing the same workflow on STM32MP157 produces a proper remote GUI, so I’m trying to understand what’s different/unsupported on i.MX91.

image (3).png

Questions

  1. Can someone please confirm whether i.MX91 (SoC + FRDM board) has no hardware display controller / no supported display outputs (HDMI/MIPI/LVDS/RGB) in the current BSP?

  2. If there is truly no display pipeline, what is the recommended approach for a headless GUI on i.MX91? For example:

    • Weston headless backend + RDP/VNC backend,

    • Xorg with Xvfb/Xdummy + xrdp,

    • or any NXP-recommended method that works with the i.MX91 graphics stack (e.g., software rendering via llvmpipe).

  3. Are there any reference designs or add-on boards for i.MX91 that provide a supported display interface? Or is display only available on other i.MX9 variants (e.g., i.MX93)?

Environment (for context)

If anyone’s interested in the exact steps I used for the RDP setup on i.MX91, I’m happy to share.

Thanks!

 

ラベル(3)
0 件の賞賛
返信
4 返答(返信)

379件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

i.MX91 FRDM only support 5-inch Tianma LCD display by default on our BSP.
Please refer to the Board User's Guide:
https://www.nxp.com/webapp/Download?colCode=UM12262&isHTMLorPDF=HTML

Chapter 3.1 5-inch Tianma LCD

Best regards/Saludos,
Aldo.

364件の閲覧回数
Zk47T
Contributor II

Hi @AldoG 

Thank you for your reply

 

Actually i know about this screen, but it so expensive, the screen price is triple the board price.

So i think i will stick with virtual display solution. Do you think it possible to some kind of port forwarding or screencast framebuffer to output GUI to xfreerdp from PC.

Also can i ask currently frdm-i.mx93 is out of stock, we need to wait at least November right ? 

0 件の賞賛
返信

351件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Yes, for stock on the freedom board please check the webpage or if urgently please contact your local NXP office or your assigned NXP sales person for any availability.

Best regards/Saludos,
Aldo.

0 件の賞賛
返信

402件の閲覧回数
Zk47T
Contributor II

Hi, anyone has any idea ? 

0 件の賞賛
返信