i.MX Yocto Project 用户指南第 LF5.10.72_2.2.0 版 — 2021 年 12 月 17 日

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Yocto Project 用户指南第 LF5.10.72_2.2.0 版 — 2021 年 12 月 17 日

Jump to solution
1,118 Views
zkyq
Contributor I

zkyq@zkyq-virtual-machine:~/GitHub/My_GitHub/NXP_IMX6ULL/build$ bitbake -k core-image-sato


NOTE: Your conf/bblayers.conf has been automatically updated.
WARNING: You have included the meta-virtualization layer, but 'virtualization' has not been enabled in your DISTRO_FEATURES. Some bbappend files may not take effect. See the meta-virtualization README for details on enabling virtualization support.
Loading cache: 100% | | ETA: --:--:--
Loaded 0 entries from dependency cache.
Parsing recipes: 100% |#############################################################################################################| Time: 0:01:36
Parsing of 3341 .bb files complete (0 cached, 3341 parsed). 4951 targets, 613 skipped, 3 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'packagegroup-core-x11-base' (but /home/zkyq/GitHub/My_GitHub/NXP_IMX6ULL/sources/poky/meta/recipes-sato/images/core-image-sato.bb RDEPENDS on or otherwise requires it)
packagegroup-core-x11-base was skipped: missing required distro feature 'x11' (not in DISTRO_FEATURES)
NOTE: Runtime target 'packagegroup-core-x11-base' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['packagegroup-core-x11-base']
ERROR: Nothing RPROVIDES 'packagegroup-core-x11-sato' (but /home/zkyq/GitHub/My_GitHub/NXP_IMX6ULL/sources/poky/meta/recipes-sato/images/core-image-sato.bb RDEPENDS on or otherwise requires it)
packagegroup-core-x11-sato was skipped: missing required distro feature 'x11' (not in DISTRO_FEATURES)
NOTE: Runtime target 'packagegroup-core-x11-sato' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['packagegroup-core-x11-sato']
ERROR: Nothing RPROVIDES 'core-image-sato'
No eligible RPROVIDERs exist for 'core-image-sato'
NOTE: Runtime target 'core-image-sato' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['core-image-sato']

 

yocto第一次编译时能完成全部过程,第二次改变机器配置后就直接报错,请问是机器配置对应的bblayers文件更新了吗?

看样子是 fsl-imx-fb 没有 X11 或 Wayland,不支持core-image-sato映像?

 

0 Kudos
Reply
1 Solution
1,087 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @zkyq 

根据的这个错误,bblayers没有所需要的layers. 不清楚你在bitbake core-image-sato之前使用的是那个DISTRO. 

Harvey021_0-1675811035495.png

MACHINE选项,你还是具体查看下conf/machine。 在看下core-image-sato.bb。

 

Best regards

Harvey

View solution in original post

0 Kudos
Reply
3 Replies
1,081 Views
Harvey021
NXP TechSupport
NXP TechSupport

可以到各个layers去查看,比如:sources/meta-imx/meta-sdk/conf/distro/

 

Best regards

Harvey

0 Kudos
Reply
1,088 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @zkyq 

根据的这个错误,bblayers没有所需要的layers. 不清楚你在bitbake core-image-sato之前使用的是那个DISTRO. 

Harvey021_0-1675811035495.png

MACHINE选项,你还是具体查看下conf/machine。 在看下core-image-sato.bb。

 

Best regards

Harvey

0 Kudos
Reply
1,082 Views
zkyq
Contributor I
fsl-imx-,手册中说明了没有X11,确实和报错对上了。但是请问有关于i.MX Yocto Project 映像更加具体的说明吗?比如能够映像支持哪些distro
0 Kudos
Reply