i.MX RT1060 Ref Manual GPIO config clarification please

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1060 Ref Manual GPIO config clarification please

ソリューションへジャンプ
1,843件の閲覧回数
philipfreidin
Contributor II

In the i.MX RT1060 Processor Reference Manual  Rev 2, on page 958, there is a column titled "SRE / SPEED Setting".

The values given are 1, 2, and 3 bits long. In the actual register where these fields are used (for example page 698) the fields are not adjacent, and SPEED is to the left of SRE.

Could someone at NXP please provide 3 bit values for this column of table 12-3, and indicate which 2 bits are SPEED and which is SRE.

Thanks.

ラベル(1)
1 解決策
1,742件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Philip,

Hope you are doing well.

The table you are referring to was made for easier reference when checking the speeds you reach, in regards to the settings configured. As you mentioned the actual register does not have them adjacent. Neither the DSE, SRE and Speed are in the order seen in the register. 

It is in ascending order first of DSE, then SRE (so this means the first four rows are when SRE = 0) and then Speed.

pastedImage_1.png

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

元の投稿で解決策を見る

1 返信
1,743件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Philip,

Hope you are doing well.

The table you are referring to was made for easier reference when checking the speeds you reach, in regards to the settings configured. As you mentioned the actual register does not have them adjacent. Neither the DSE, SRE and Speed are in the order seen in the register. 

It is in ascending order first of DSE, then SRE (so this means the first four rows are when SRE = 0) and then Speed.

pastedImage_1.png

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------