i.MX RT1050 GPIO output type?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1050 GPIO output type?

ソリューションへジャンプ
1,695件の閲覧回数
audio
Contributor III

Hello,

I have been looking at the MX RT1050 Datasheet, but I wasn't able to find a clear question to my question. 

Does MX RT1050 GPIO support both Push pull(CMOS) and open drain configuration?

On pg.32, there are electrical specs. for multiple pull up and pull down resistor values, but I couldn't find any explicit words that MX RT1050 supports both Push pull and open drain.

Could anyone help me out clarifying this? If both settings are configurable, where do I configure it?

 

Best Regards,

0 件の賞賛
返信
1 解決策
1,678件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Yes, i.MX RT1050 supports both CMOS and Open Drain configuration. You can enable Open Drain using ODE bit in IOMUXC_SW_PAD_CTL_PAD register. Please check the below snippet from the reference manual. For more information please check the GPIO chapter in RM.

image.png

Best regards,

Felipe

元の投稿で解決策を見る

1 返信
1,679件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Yes, i.MX RT1050 supports both CMOS and Open Drain configuration. You can enable Open Drain using ODE bit in IOMUXC_SW_PAD_CTL_PAD register. Please check the below snippet from the reference manual. For more information please check the GPIO chapter in RM.

image.png

Best regards,

Felipe