i.MX RT series data conversion from SPDIF to I2S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT series data conversion from SPDIF to I2S

978 Views
audio
Contributor III

Hello,

 

I have the codes for receiving SPDIF input and I2S output on i.MX RT processors, but I'm trying to find if there's any standard or most optimized way of converting the data for i.MX RT processors. Could anyone share if there's any documents or code examples which does the conversion?

 

Best regards

Brian

0 Kudos
Reply
1 Reply

973 Views
art
NXP Employee
NXP Employee

There is no any internal hardware interconnection between SPDIF and SAI modules
inside i.MX RT SoCs. So, the only way to transfer audio from SPDIF to SAI is to
receive data from SPDIF, buffer them into memory and then send them to SAI
under software control, possibly, using DMA.

Best Regards,

Artur

0 Kudos
Reply