Hello,
I am having troubles booting from SPI NOR device on an iMX6DL processor.
When I read ROM Event log buffer, I get the code 0x090000: Image authentication result, with status 0x000A0533, which is not documented in AN12853.
Can someone help me with that specific error code ?
Thanks
Camille
Solved! Go to Solution.
Hi @CamilleL ,
I hope you are doing well.
We will inform our documentation team for AN12853 to update this ROMs Log event,
If there are no further queries, can I mark this case as close?
Thanks & Regards,
Sanket Parekh
Hello Sanket,
Thanks for your help.
We finaly found that our problem is not software, it is hardware.
We didn't find yet the root cause, but it is linked to perturbations on the SPI bus.
The behavior we encounterwith this error code is a side effect.
Anyway, thanks for the informations.
It could be nice to update the AN12853.
Regards
Camille
Hi @CamilleL ,
I hope you are doing well.
We will inform our documentation team for AN12853 to update this ROMs Log event,
If there are no further queries, can I mark this case as close?
Thanks & Regards,
Sanket Parekh