i.MX Pins Tool Verions 2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Pins Tool Verions 2.0

1,363 Views
nagamaheshg
Contributor III

Dear Team,

We are doing pin mux for phyCORE-i.MX6UL, so I downloaded the pin mux tool from the below link which is i.MX Pins Tool Verions 3.0.2:

Pins Tool for i.MX Application Processors|NXP 

But the below ".mex" file is made for i.MX Pins Tool Verions 2.0:

ftp://ftp.phytec.de/pub/Products/phyBOARD-Segin-iMX6UL/TechData/MCIMX6G2VM.mex

So, could please share the Download link for i.MX Pins Tool Verions 2.0.

Regards

Nagamahesh Gamidi

Labels (1)
3 Replies

1,020 Views
Yuri
NXP Employee
NXP Employee

Hello,

Pins Tool for i.MX Application Processors|NXP 

Summary Page :

i.MX Software and Development Tools|NXP 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos

1,020 Views
nagamaheshg
Contributor III

Hi Yuri,

The below link is helpful to me.

http://www.nxp.com/downloads/en/software/Pins_Tool_for_i.MX_Processors_v2_x64_online_b161010.exe 

Thank you very much.

Regards

Nagamahesh Gamidi

0 Kudos

1,020 Views
jan_spurek
NXP Employee
NXP Employee

Hello Nagamahesh,

as stated in the dialog window in your screenshot, .mex file made in v2.0 can be opened in v3.0 without a problem.

If you have no other reason to use v2.0, it is recommended to use the latest version of the tool.

Best Regards,

Jan