Hello everyone,
I have a i.MX 8XLite Evaluation Kit(MCIMX8DXL-WEVK, SCH-54318 REV A3). Now, there is
some questions: 1、if boot from SD card,it will power down and up cyclical about 300 milliseconds.
2、serial download mode,when insert USB typ C(J15),PC show "LIBUSB_ERROR_IO" by uuu download.
Solved! Go to Solution.
Hi @jackchen1,
I have the same problem.
I downloaded LF_v6.1.36-2.1.0_images_IMX8DXLEVK.zip and I mounted on SD card "imx-image-full-imx8dxlevk.wic" (7GB size)
.When I plug the SD card and I switch on the board, led D3 start blinking (I suppose it is resetting continously).
Dip switches of SW1 are set to 1101.
i don't see any data on the serial port. I only see COM port 12-13-14-15 even if the board is powered off.
Hi @jackchen1,
Hi @jackchen1,