i.MX 8MQuad Evaluation kit boot-up issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8MQuad Evaluation kit boot-up issue

1,709 Views
neel_desai
Contributor I

Hi,

Currently, I have working on i.MX 8M Quad Evaluation Kit. I have create one layer and add new machine in yocto. Now I try to flash evk board using below command.

sudo ./uuu -b emmc_all imx-boot-<machine>-sd.bin-flash_evk < custom bz2 image> 

Output: 

Success 1 Failure 0

uuu Flashing Log:

1:2>Start Cmd:FB: ucmd setenv fastboot_dev mmc
1:2>Okay (0.02s)
1:2>Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}
1:2>Okay (0.589s)
1:2>Start Cmd:FB: ucmd mmc dev ${emmc_dev}
1:2>Okay (0.213s)
1:2>Start Cmd:FB: flash -raw2sparse all /home/neel75/Downloads/LF_v5.4.y-1.0.0_images_MX8MQEVK/imx-image-full-imx8mqevk.sdcard
100%1:2>Okay (542.1s)
1:2>Start Cmd:FB: flash bootloader /home/neel75/Downloads/LF_v5.4.y-1.0.0_images_MX8MQEVK/imx-boot-imx8mqevk-sd.bin-flash_evk
0x400000001:2>Okay (0.422s)
1:2>Start Cmd:FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
1:2>Okay (0.011s)
1:2>Start Cmd:FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
1:2>Okay (0.013s)
1:2>Start Cmd:FB: done
1:2>Okay (0s)

Flashing Log on UART:

downloading of 1487560 bytes finished
request 00000000fdccb800 was not queued to ep1in-bulk
writing to partition 'bootloader'
Initializing 'bootloader'
switch to partitions #1, OK
mmc0(part 1) is current device
Writing 'bootloader'

MMC write: dev # 0, block # 66, count 2906 ... 2906 blocks written: OK
Writing 'bootloader' DONE!
request 00000000fdccb800 was not queued to ep1in-bulk
Detect USB boot. Will enter fastboot mode!
request 00000000fdccb800 was not queued to ep1in-bulk
Detect USB boot. Will enter fastboot mode!
request 00000000fdccb800 was not queued to ep1in-bulk

 

Observation:

1. Evk not boot-up in internal boot mode

2. I have flashed pribuilt image in evk but not boot-up in internal boot mode.

Question:

Please give the suggestion for this issue.

0 Kudos
Reply
3 Replies

1,639 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using? Are you using the demo images or images you build yourself?

0 Kudos
Reply

1,639 Views
neel_desai
Contributor I

Hi Rita,

First I have flashed the (LF_v5.4.y-1.0.0) demo image in i.MX8M Quad Evk and board boot up successfully.

After that i have create custom layer in yocto and build the custom images.

I have flashed the custom images but system doesn't boot-up. After that I have flashed demo images but board not boot-up.

0 Kudos
Reply

1,639 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For the demo images can work, we have tested on our board. You make sure the boot mode and boot command are right. You can retry it.

0 Kudos
Reply