i.MX 8MQuad EVK, DDR density change

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8MQuad EVK, DDR density change

1,282 Views
jekim
Contributor III

Hello,

My board (i.MX 8MQuad EVK) has one 3GB (768Meg x 32) LPDDR4 IC. DISTRO is L4.9.88_2.0.0 version.

If I depopulate the RAM and populate another IC with bigger or smaller density than 3GB, how can I configure this change? Is there any limitation for allowed density size on my board?

Best Regards,

Jeff

Labels (1)
Tags (1)
0 Kudos
4 Replies

1,102 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeff

please check ddr tool on below link and Chapter 4 How to bring up a new MX8M board MX8M_DDR_Tool_User_Guide.docx included in package.
i.MX 8M DDR Tool Release 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,102 Views
jekim
Contributor III

Hi igor,

Thank you for reply. I've tried to modify the excel file "MX8M_LPDDR4_register_programming_aid_EVK_preliminiary_v16.xlsx" to generate new script file for DDR tool.

When I change density related parameters on top table, I see connected ADDRMAP* registers are changed accordingly.

Btw, which source program file defines these register values?

Best Regards,

Jeff

0 Kudos

1,102 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeff

 

seems this is described on p. 11 MX8M_DDR_Tool_User_Guide.docx included in package.

pastedImage_1.jpg

 

Best regards
igor

1,102 Views
jekim
Contributor III

Hi igor,

Thanks. I will generate script file for different DDR densities by "MX8M_LPDDR4_register_programming_aid_EVK_preliminiary_v16.xlsx". DDR tool would generate updated c-program source from the script files I guess.

Best Regards,

Jeff

0 Kudos