Hi,
I'm running yocto on an sd card in the Google Coral platform.
We are developing a program that works fine otherwise, but after running for a few minutes the display that is connected to the coral shows a couple of kernel messages and the entire system freezes until power is cut by unplugging the system.
The kernel messages that appear are either of the following:
#1:
buck3: failed to disable
imx8m_gpc_pm_domain gpc_power_domain@4: failed to power off the reg-110
#2:
buck3: failed to disable
cpu cpu0: failed to scale dc_reg up: -11
imx8m_gpc_pm_domain gpc_power_domain@4 : failed to power off the reg-11
cpufreq: __target_index: Failed to change cpu frequency: -11
Could this be related to having not set some kernel flags?
Hi Milan
from log "cpufreq: __target_index: Failed to change cpu frequency" issue may be related
to cpufreq driver so one can check sect.2.5.3 CPU Frequency Scaling (CPUFREQ)
Also issue may be posted on coral support https://coral.ai/software/
Best regards
igor