i.MX 8M mini secure boot with yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8M mini secure boot with yocto

1,336件の閲覧回数
aditi1prakash
Contributor I

Dear NXP community,

I am trying to perform secure boot operation with yocto project on i.MX 8M Mini hardware. Following are the software details. 

I am able to successfully build the yocto project without secure boot but I have few questions regarding the process of achieving secure boot using yocto project.

  1. Does NXP provide a layer (/recipes) to enable secure boot with Yocto?
  2. Or, do we need to configure our own recipe manually?
  3. If yes, is there a guide or reference document/templates available for the same?

Regards,

Aditi Prakash

iMX8MMINI

0 件の賞賛
返信
2 返答(返信)

1,247件の閲覧回数
aditi1prakash
Contributor I

Thanks @Harvey021.

I had a couple of follow-up questions:

  • Is there a recommended third-party layer that can sort of act as plug-and-play (or that can be integrated with minimal efforts) with NXP yocto project? Because many that I referred to (variscite, digi-embedded..) offer their own hardware based on i.MX for their software.
  • What would be the approximate effort to write these recipes on my own? (with basic knowledge of yocto project)

Regards,

Aditi Prakash

0 件の賞賛
返信

1,301件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi @aditi1prakash 

As I know, we've not had such support with Yocto so far. 

 

Best regards

Harvey