i.MX 8M Quad SMP multicore operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8M Quad SMP multicore operation

1,252件の閲覧回数
anhui527
Contributor III

Hi, I want to use i.MX 8M Quad with u-boot only, to run a task in SMP mode multicore? Which steps I should do to enable this mode? Which part of u-boot needs to be modified?#i.MX 8M Quad

0 件の賞賛
返信
1 返信

1,180件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi An

I am afraid this is not supported in nxp uboot releases and may be posted on

uboot mail list U-Boot Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信